2019-02-28 12:37 PM
Hi everybody!
I working on a simple project but with some sensors and co.
I'm newbie with the STM32 and I want to try to port the project from the ATmega2560 to the STM32.
But witch chip?
I need :
> SPI for an TFT screen 2.2" (ILI9340C or ILI9341)
> SPI for a MicroSD Card
> BMP180 sensor
> 2 pins interup
> 3 indepedants Pins PWM
> 2 ADC
> RTC time
> One Serial for bluetooth HC-05
> One Serial for an GPS L80
> One Serial for connect an external probe
> 10 digital Input
> 4 digital Output
> min 72Mhz for the sreen
> All pin in 3.3v
Question :
> Minimum 64K of program space ?
> Flashing the MPU directly with the USB port ?
> Possible to program all from the Arduino IDE ? ( with the right card )
Thanks!
Solved! Go to Solution.
2019-02-28 02:23 PM
Play with the MCU selector.
2019-02-28 02:23 PM
Play with the MCU selector.
2019-03-22 04:06 PM
The cheap STM32F103 should manage that. Google for Blue Pill as a suitable test bed.