cancel
Showing results for 
Search instead for 
Did you mean: 

Why are we getting the error Boot over usb0! DSI version 0x0 not supported Invalid or missing layout file.DFU alt info setting: done crq->brequest:0x0

GeorgeR
Associate II
Loading Environment from MMC... OK
In:    serial
Out:   serial
Err:   serial
stm32 vrefbuf timed out: -110
adc@0: can't enable vdd-supply!adc_measurement: single shot failed for adc@0[18]!
Net:   eth0: ethernet@5800a000
Hit any key to stop autoboot:  0
Boot over usb0!
DSI version 0x0 not supported
Invalid or missing layout file.DFU alt info setting: done

We can successfully load the StarterPackage FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv, but when we try creating from Developer Package, we get this error.

Our board has a STM32MP151CAC. We have been testing on the STM32MP157F-DEV2, on which there has been no problem.

Is there a default for booting over USB, and not the SD?

Thanks in advance,

George

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Olivier GALLIEN
ST Employee

Hi @GeorgeR​ ,

I understand trace you provide come from console while flashing with CubeProg right ?

>>Our board has a STM32MP151CAC. We have been testing on the STM32MP157F-DEV2, on which >> there has been no problem.

MP151C and MP157F can not boot with same BSP settings. Device Tree have to be adapted.

Can you please provide :

  • Complete console log
  • tsv file you are trying to load
  • DT files you embed in "developer package"

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.