cancel
Showing results for 
Search instead for 
Did you mean: 

spi-nand flash layout download failed with CubeMXProgrammer

ASkri.1
Senior

Hi, ST :)

In addition to https://community.st.com/s/question/0D53W00000pUh4gSAC/tfa-and-uboot-custom-compile-fails

Could you plese explain me what is the reason for such error:

dfu_fill_entity_mtd: Memory layout (/0x10/1*122Me) not supported!

while downloading flash content with CubeMXProgrammer.

I've built a core image with bitbake st-image-core command (hope I'm correct here) and got UBI image with size 116Mb (121896960b). I'm expecting it can be fitted to a UBI partition that has size 0x07a00000b = 127926272b. Please refer to nand partition table below. spi-nand flash size is 128Mb.

TF-A and u-boot was manually build during duscussion mentioned with link above.

Here is .tsv file:

#Opt Id Name Type IP Offset Binary

- 0x01 fsbl-boot Binary none 0x0 ./tf-a-stm32mp157a-stm32mp151-dk1-mx-usb.stm32

- 0x03 fip-boot Binary none 0x0 ./fip-stm32mp157a-stm32mp151-dk1-mx-trusted.bin

P 0x04 fsbl Binary(2) spi-nand0 0x000000 ./tf-a-stm32mp157a-stm32mp151-dk1-mx-nand.stm32

P 0x05 fip1 Binary spi-nand0 0x200000 ./fip-stm32mp157a-stm32mp151-dk1-mx-trusted.bin

P 0x06 fip2 Binary spi-nand0 0x400000 ./fip-stm32mp157a-stm32mp151-dk1-mx-trusted.bin

P 0x10 UBI Binary spi-nand0 0x600000 ./st-image-core-openstlinux-weston-stm32mp1-duck_nand_4_256_multivolume.ubi

Here is exact console output:

Here is console full output while CubeMX programming (one more question after log):

-----------------------

NOTICE: CPU: STM32MP157DAB Rev.Z

NOTICE: Model: STMicroelectronics STM32MP157A-DK1 STM32CubeMX board

INFO:  Reset reason (0x15):

INFO:   Power-on Reset (rst_por)

INFO:  PMIC version = 0x21

INFO:  FCONF: Reading TB_FW firmware configuration file from: 0x2ffe3000

INFO:  FCONF: Reading firmware configuration information for: stm32mp_io

INFO:  Using USB

INFO:   Instance 2

INFO:  Boot used partition fsbl1

NOTICE: BL2: v2.4-r1.0(debug):

NOTICE: BL2: Built : 13:28:40, Jun 2 2021

INFO:  BL2: Doing platform setup

INFO:  RAM: DDR3-DDR3L 16bits 533000Khz

WARNING: Couldn't find property st,phy-cal in dtb

INFO:  Memory size = 0x20000000 (512 MB)

INFO:  DFU USB START...

INFO:  phase ID :0, Manifestation 0 at c00001dc

INFO:  phase ID :3, Manifestation 3 at c80feb64

INFO:  Send detach request

INFO:  Receive DFU Detach

INFO:  DFU USB STOP...

INFO:  BL2: Loading image id 31

INFO:  Loading image id=31 at address 0x2ffff000

WARNING: Image id=31 size out of bounds

ERROR: BL2: Failed to load image id 31 (-27)

NOTICE: CPU: STM32MP157DAB Rev.Z

NOTICE: Model: STMicroelectronics STM32MP157A-DK1 STM32CubeMX board

INFO:  Reset reason (0x14):

INFO:   Pad Reset from NRST

INFO:  PMIC version = 0x21

INFO:  FCONF: Reading TB_FW firmware configuration file from: 0x2ffe3000

INFO:  FCONF: Reading firmware configuration information for: stm32mp_io

INFO:  Using USB

INFO:   Instance 2

INFO:  Boot used partition fsbl1

NOTICE: BL2: v2.4-r1.0(debug):

NOTICE: BL2: Built : 13:28:40, Jun 2 2021

INFO:  BL2: Doing platform setup

INFO:  RAM: DDR3-DDR3L 16bits 533000Khz

WARNING: Couldn't find property st,phy-cal in dtb

INFO:  Memory size = 0x20000000 (512 MB)

INFO:  DFU USB START...

INFO:  phase ID :0, Manifestation 0 at c00001dc

INFO:  phase ID :3, Manifestation 3 at c80f9ea3

INFO:  Send detach request

INFO:  Receive DFU Detach

INFO:  DFU USB STOP...

INFO:  BL2: Loading image id 31

INFO:  Loading image id=31 at address 0x2ffff000

INFO:  Image id=31 loaded: 0x2ffff000 - 0x2ffff226

INFO:  FCONF: Reading FW_CONFIG firmware configuration file from: 0x2ffff000

INFO:  FCONF: Reading firmware configuration information for: dyn_cfg

INFO:  FCONF: Reading firmware configuration information for: stm32mp1_firewall

INFO:  BL2: Loading image id 4

INFO:  Loading image id=4 at address 0x2ffc5000

INFO:  Image id=4 loaded: 0x2ffc5000 - 0x2ffd847c

WARNING: Not a known TEE, use default loading options.

INFO:  BL2: Skip loading image id 21

INFO:  BL2: Skip loading image id 22

INFO:  BL2: Loading image id 23

INFO:  Loading image id=23 at address 0xc0500000

INFO:  Image id=23 loaded: 0xc0500000 - 0xc0512a91

INFO:  BL2: Loading image id 26

INFO:  Loading image id=26 at address 0x2ffc0000

INFO:  Image id=26 loaded: 0x2ffc0000 - 0x2ffc4258

INFO:  BL2: Loading image id 5

INFO:  Loading image id=5 at address 0xc0100000

INFO:  Image id=5 loaded: 0xc0100000 - 0xc01cfa18

NOTICE: BL2: Booting BL32

INFO:  Entry point address = 0x2ffc5000

INFO:  SPSR = 0x1d3

NOTICE: SP_MIN: v2.4-r1.0(debug):

NOTICE: SP_MIN: Built : 15:20:23, Jun 2 2021

INFO:  ARM GICv2 driver initialized

INFO:  Set calibration timer to 60 sec

INFO:  ETZPC: UART1 (3) could be non secure

INFO:  ETZPC: SPI6 (4) could be non secure

INFO:  ETZPC: CRYP1 (9) could be non secure

INFO:  ETZPC: I2C6 (12) could be non secure

INFO:  SP_MIN: Initializing runtime services

INFO:  SP_MIN: Preparing exit to normal world

U-Boot 2020.10-stm32mp-r1 (Jun 02 2021 - 18:21:14 +0300)

CPU: STM32MP157DAB Rev.Z

Model: STMicroelectronics STM32MP157A-DK1 STM32CubeMX board

Board: stm32mp1 in trusted - stm32image mode (st,stm32mp157a-stm32mp151-dk1-mx)

DRAM: 512 MiB

Clocks:

- MPU : 800 MHz

- MCU : 208.878 MHz

- AXI : 266.500 MHz

- PER : 24 MHz

- DDR : 533 MHz

WDT: Started with servicing (32s timeout)

NAND: 0 MiB

MMC: STM32 SD/MMC: 0

In:  serial

Out: serial

Err: serial

invalid MAC address in OTP 00:00:00:00:00:00

stm32 vrefbuf timed out: -110

adc@0: can't enable vdd-supply!adc_measurement: single shot failed for adc@0[18]!

Net:

Error: ethernet@5800a000 address not set.

No ethernet found.

Hit any key to stop autoboot: 0

Boot over usb0!

partitions : done

DFU alt info setting: using id 'spi-nand0,0'

using id 'spi-nand0,1'

using id 'spi-nand0,2'

dfu_fill_entity_mtd: Memory layout (/0x10/1*122Me) not supported!

Error: dfu init failed: -1

done

STM32MP> mtdparts

device spi-nand0 <spi-nand0>, # parts = 4

 #: name        size      offset     mask_flags

 0: fsbl        0x00200000   0x00000000   0

 1: ssbl1       0x00200000   0x00200000   0

 2: ssbl2       0x00200000   0x00400000   0

 3: UBI        0x07a00000   0x00600000   0

active partition: spi-nand0,0 - (fsbl) 0x00200000 @ 0x00000000

defaults:

mtdids : spi-nand0=spi-nand0

mtdparts: mtdparts=spi-nand0:2m(fsbl),2m(ssbl1),2m(ssbl2),-(UBI)

-----------------------

BTW, I'm also not able to load 0x04,0x05,0x6 partitions without specifying 0x10 partition with following error:

Boot over usb0!

Error: fip2 (0x6): Bad size for partition 3 (ssbl2) at 0x400000 = 0x7c00000 <> 0x200000 expected

Here is .tsv (last line is commented):

#Opt Id Name Type IP Offset Binary

- 0x01 fsbl-boot Binary none 0x0 ./tf-a-stm32mp157a-stm32mp151-dk1-mx-usb.stm32

- 0x03 fip-boot Binary none 0x0 ./fip-stm32mp157a-stm32mp151-dk1-mx-trusted.bin

P 0x04 fsbl Binary(2) spi-nand0 0x000000 ./tf-a-stm32mp157a-stm32mp151-dk1-mx-nand.stm32

P 0x05 fip1 Binary spi-nand0 0x200000 ./fip-stm32mp157a-stm32mp151-dk1-mx-trusted.bin

P 0x06 fip2 Binary spi-nand0 0x400000 ./fip-stm32mp157a-stm32mp151-dk1-mx-trusted.bin

#P 0x10 UBI Binary spi-nand0 0x600000 ./st-image-core-openstlinux-weston-stm32mp1-duck_nand_4_256_multivolume.ubi

This migh be convinient for TF-A/U-BOOT debugging - no need to wait for download huge images...

Thank you for your patience :)

Looking forward for your reply

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Hi, Oliver! No... There was a simple reason I've discovered. mtd partitions in u-boot and in .tsv file were different. tsv file - 2Mb-2Mb-2Mb-UBI u-boot config - 2Mb-4Mb-4Mb-UBI So, this question is considered to be closed. Thank you very much. пн, 7 июн. 2021 г. в 15:40, ST Community :

View solution in original post

2 REPLIES 2
Olivier GALLIEN
ST Employee

Hi @ASkri.1​ ,

Sorry I'm not expert of nand and mtd but the mention trace

dfu_fill_entity_mtd: Memory layout (/0x10/1*122Me) not supported!

looks to be obvious

Look inside u-boot source "drivers/dfu/dfu_mtd.c"

if ((!strcmp(st, "part")) || (!strcmp(st, "partubi"))) { 
...
}
else {
 
		printf("%s: Memory layout (%s) not supported!\n", __func__, st);
 
		return -1;
 
	}

I understand you provide one parameter as "/0x10/1*122Me" where it expect to find "part" or "partubi"

Hope this help

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Hi, Oliver! No... There was a simple reason I've discovered. mtd partitions in u-boot and in .tsv file were different. tsv file - 2Mb-2Mb-2Mb-UBI u-boot config - 2Mb-4Mb-4Mb-UBI So, this question is considered to be closed. Thank you very much. пн, 7 июн. 2021 г. в 15:40, ST Community :