2024-05-08 3:34 AM - last edited on 2024-07-08 4:42 AM by Amel NASRI
Dear. All.
I have one problem.
until now, I used well to connect with USB OTG interface.
I've been using USB C to USB A cable. and then, we have no problem.
but, I found a problem at using USB C to USB C connectivity.
the PC & my MP151C board didn't recognize each other.
I'll use my device for slave.
our circuit as bellow.
thank you.
2024-07-08 5:32 AM
ID pin is useless for USB Type-C, the concept does not exist.
CC1/CC2 lines should have each a 5.1K pull-dow to be recognized as a slave device by the Host PC.
Regards.