cancel
Showing results for 
Search instead for 
Did you mean: 

USB C connection problem with MP151cad3.

Geonbangjini
Associate

Dear. All.

I have one problem.

until now, I used well to connect with USB OTG interface.

I've been using USB C to USB A cable. and then, we have no problem.

but, I found a problem at using USB C to USB C connectivity.

the PC & my MP151C board didn't recognize each other.

I'll use my device for slave.

our circuit as bellow.

thank you.

Geonbangjini_0-1715164396958.png

 

1 REPLY 1
PatrickF
ST Employee

Hi @Geonbangjini 

ID pin is useless for USB Type-C, the concept does not exist.

CC1/CC2 lines should have each a 5.1K pull-dow to be recognized as a slave device by the Host PC.

 

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.