cancel
Showing results for 
Search instead for 
Did you mean: 

Support for BlueZ in the STM32MPU distribution package?

darla14
Senior

Hello ,

Is the BlueZ supported or added in the Distribution or developer or starter image?

I tried running bluetoothd -v to get the version of the bluetoothd (and hence the Bluez which has this demon built) but I got this :

root@stm32mp1:~# bluetoothd -v

-sh: bluetoothd: not found

I then tried building the Distribution package which has this meta-connectivity layer where there is BlueZ is in add on Recipes ( https://wiki.st.com/stm32mpu/wiki/STM32MP15_OpenSTLinux_release_note)

bluez5meta-st/meta-st-openstlinux/recipes-connectivity/bluez5/bluez5_%.bbappend

Do I have to add this layer? or will it be built by bitbake st-image-weston

?

 Using bitbake st-image-weston and fishing the image gives the same result.

Please tell the steps to build and use BlueZ and all the utilities it provides (bluetoothd,meshctl)

Thanks in advance !

Regards,

D

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Hi @darla14​ 

first, you need to check if your BT environment is correctly probed: https://wiki.st.com/stm32mpu/wiki/Bluetooth_overview#How_to_trace_and_debug_the_framework

From my side, after setting the BT parameters (https://wiki.st.com/stm32mpu/wiki/How_to_set_up_a_Bluetooth_connection) and following this wiki page https://wiki.st.com/stm32mpu/wiki/How_to_scan_Bluetooth_devices, I successfully paired my board STM32MPU157C-DK2 running OpenSTLinux 3.0 with my phone.

For BTLE, take a look at the wiki page https://wiki.st.com/stm32mpu/wiki/How_to_scan_BLE_devices#BLE_device_connection_step-by-step

Finally, the error message you referred to is normal as the BT daemon is already running through the systemd service:

$ systemctl status bluetooth
[0;1;32m*[[0m bluetooth.service - Bluetooth service
     Loaded: loaded (/lib/systemd/system/bluetooth.service; enabled; vendor preset: enabled)
     Active: [[0;1;32mactive (running)[[0m since Tue 2021-08-31 08:09:42 UTC; 2min 35s ago
       Docs: man:bluetoothd(8)
   Main PID: 571 (bluetoothd)
     Status: "Running"
     Memory: 2.0M
     CGroup: /system.slice/bluetooth.service
             `-571 /usr/libexec/bluetooth/bluetoothd
 
Aug 31 08:09:41 stm32mp1 systemd[1]: Starting Bluetooth service...
Aug 31 08:09:42 stm32mp1 systemd[1]: Started Bluetooth service.

Best regards,

--JM

View solution in original post

9 REPLIES 9
Jean-Marc B
ST Employee

Hi @darla14​ 

Bluetooth is fully supported and the bluetoothd program is installed by default in OpenSTLinux image but it is not available in your PATH environment:

root@stm32mp1:~# ps -aux | grep blue
root       572  0.0  0.6   4792  2920 ?        Ss   06:31   0:00 /usr/libexec/bluetooth/bluetoothd
root      1100  0.0  0.2   2024  1112 ttySTM0  S+   06:37   0:00 grep blue

So, the command you mentioned runs fine:

root@stm32mp1:~# /usr/libexec/bluetooth/bluetoothd -v
5.55

About the availability of the meshctl utility, please refer to the following link : https://community.st.com/s/question/0D50X0000BTdF20SQF/stm32mp157cdk2-bluetooth-mesh .

Best regards,

--JM

Edit: add link to build meshctl

darla14
Senior

Thanks for your reply. Do you know where I can find the compiled binary for

https://github.com/bluez/bluez/blob/master/test/example-gatt-server ??

or

https://github.com/bluez/bluez/blob/master/tools/gatt-service.c

Regards,

D

Hi @darla14​ 

The two binaries are available from the package bluez5-testtools from our OpenSTLinux repository. You can install it with the command:

$ apt-get install bluez5-testtools

The compiled binaries are then in the directory /usr/lib/bluez/test

Best regards,

--JM

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'.

Thanks for the prompt reply .

Ok this works , after i did apt-get update as well before running

apt-get install bluez5-testtools

root@stm32mp1:/usr/lib/bluez/test# ./example-gatt-server 

./example-gatt-server:394: PyGIDeprecationWarning: GObject.timeout_add is deprecated; use GLib.timeout_add instead

 GObject.timeout_add(5000, self.drain_battery)

./example-gatt-server:651: PyGIDeprecationWarning: GObject.MainLoop is deprecated; use GLib.MainLoop instead

 mainloop = GObject.MainLoop()

Registering GATT application...

GetManagedObjects

GATT application registered

But on the lightblue App (iPhone) , i cant see the device.What device name should I get?

Also is there way to build this using makefile if I want to customise it? How?

Since it depends on dbus and glib and bluez requires ./confgue kind of scripts to build which I am not sure is feasible for cross compiling the bluez/test-*

Regards,

D

Hi @darla14​ 

I am glad you resolve your initial problems!

About the bluetooth usage, I recommand the following wiki : https://wiki.st.com/stm32mpu/wiki/Bluetooth_overview and its derivative pages.

For the development of applications, this wiki page https://wiki.st.com/stm32mpu/wiki/How_to_cross-compile_with_the_Developer_Package may help you.

Best regards,

--JM

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'.

Hello @Jean-Marc B​ ,

Thanks for the reply,

I am able to cross compile the utilities and run it on stm32mp1 but strangely I think I may have to enable something else .Is the bluetooth low energy enabled by default?If not what commands is needed to turn it on.

As a test I ran bluetoothctl and then scan on and I got this ,I rebooted as well :

[bluetooth]# scan on

Failed to start discovery: org.bluez.Error.NotReady

list command shows the default the MAC address :

[bluetooth]# list

Controller 43:43:A1:12:1F:AC stm32mp1 [default]

Also :

/usr/libexec/bluetooth# ./bluetoothd 

D-Bus setup failed: Name already in use

Can you please tell whats wrong here?

Regards,

Hi @darla14​ 

first, you need to check if your BT environment is correctly probed: https://wiki.st.com/stm32mpu/wiki/Bluetooth_overview#How_to_trace_and_debug_the_framework

From my side, after setting the BT parameters (https://wiki.st.com/stm32mpu/wiki/How_to_set_up_a_Bluetooth_connection) and following this wiki page https://wiki.st.com/stm32mpu/wiki/How_to_scan_Bluetooth_devices, I successfully paired my board STM32MPU157C-DK2 running OpenSTLinux 3.0 with my phone.

For BTLE, take a look at the wiki page https://wiki.st.com/stm32mpu/wiki/How_to_scan_BLE_devices#BLE_device_connection_step-by-step

Finally, the error message you referred to is normal as the BT daemon is already running through the systemd service:

$ systemctl status bluetooth
[0;1;32m*[[0m bluetooth.service - Bluetooth service
     Loaded: loaded (/lib/systemd/system/bluetooth.service; enabled; vendor preset: enabled)
     Active: [[0;1;32mactive (running)[[0m since Tue 2021-08-31 08:09:42 UTC; 2min 35s ago
       Docs: man:bluetoothd(8)
   Main PID: 571 (bluetoothd)
     Status: "Running"
     Memory: 2.0M
     CGroup: /system.slice/bluetooth.service
             `-571 /usr/libexec/bluetooth/bluetoothd
 
Aug 31 08:09:41 stm32mp1 systemd[1]: Starting Bluetooth service...
Aug 31 08:09:42 stm32mp1 systemd[1]: Started Bluetooth service.

Best regards,

--JM

Thanks , it helped.I will test further !

Regards

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.