cancel
Showing results for 
Search instead for 
Did you mean: 

STMprogrammers ends inmedialty and do not flash eMMC

Jroch.1
Associate II

Hello

A STM32MP15 device

if flahs proccess is started with STMCube programmer, the proccess finished inmediatly saying "process sucessfull" so the device is not booting , in eMMC mode or SD mode

1 REPLY 1
Olivier GALLIEN
ST Employee

Hi @Jroch.1​ ,

Are you still facing the issue ?

If yes, could you please share :

  • ecosystem version you are using and CubeProg version
  • content of the tsv you are flashing
  • custom or ST board ?
  • Log/trace of both cubeprog and board console.( UART4)

Thx

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.