cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP157F-DK2: Boot from USB SSD Instead of SD Card

symeon
Associate II

Hello everyone,

I would like to ask if it is possible to configure the STM32MP157F-DK2 to boot from a USB SSD instead of an SD card. If so, could you please share the steps or documentation?

Thank you in advance!

Best regards,
Symeon Zapsis

1 ACCEPTED SOLUTION

Accepted Solutions
PatrickF
ST Employee

Hi @symeon 

The STM32MP157F-DK2 always need to do low level boot from SD-Card (other boot interface such as Serial-NOR, Serial-NAND, eMMC or SLC-NAND are not available on this boarD).
The STM32MP1 does not have any way to boot from USB device such as external drive.

Only option is to put TF-A and uBoot on SD-card which will load the kernel from an USB drive.

I'm not expert and I don't know how this is easy or complex to do and if there is bootleneck (e.g. having USB host driver in uBoot).

Regards.

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
PatrickF
ST Employee

Hi @symeon 

The STM32MP157F-DK2 always need to do low level boot from SD-Card (other boot interface such as Serial-NOR, Serial-NAND, eMMC or SLC-NAND are not available on this boarD).
The STM32MP1 does not have any way to boot from USB device such as external drive.

Only option is to put TF-A and uBoot on SD-card which will load the kernel from an USB drive.

I'm not expert and I don't know how this is easy or complex to do and if there is bootleneck (e.g. having USB host driver in uBoot).

Regards.

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Dear @PatrickF 

Thank you for your answer.

Best Regards.

Symeon Zapsis