cancel
Showing results for 
Search instead for 
Did you mean: 

[stm32mp157D] Two board have different number of cpu when I use lscpu

MJo.3
Associate II

Hi,
I bought two same board and use one to test.
After upgrade stlinux on this testing board, the cpu it can recognize is only one when the other one can recognize it two.
could you give me a guide to fix it and why this happened?

Thanks.

1 ACCEPTED SOLUTION

Accepted Solutions
Olivier GALLIEN
ST Employee

Hi @MJo.3 ,

 

I also notice difference in OPP_MODE 

 

So I'm wondering if you have same software version embed in the 2 boards

 

Can you share boot logs of each boards ? 

 

Thanks 

 

Olivier 

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Olivier GALLIEN
ST Employee

Hi @MJo.3 ,

 

I also notice difference in OPP_MODE 

 

So I'm wondering if you have same software version embed in the 2 boards

 

Can you share boot logs of each boards ? 

 

Thanks 

 

Olivier 

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

I checked software version and it's not same.

I upgrade the os, and it works

 

Thanks