2019-07-18 6:11 AM
I've tried to flash STM32MP157C-DK2 SDCard like described in ST wiki with command STM32_Programmer_CLI -c port=usb1 -w flashlayout_st-image-weston/FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv.
and it didn't work! i got following error report. it seems it has trouble to reconnect the device. does anyone have an idea why it didn't work? or does anybody get similar problem? how do i get it working? Thanks a lot!
-------------------------------------------------------------------
STM32CubeProgrammer v2.1.0
-------------------------------------------------------------------
USB speed : Full Speed (12MBit/s)
Manuf. ID : STMicroelectronics
Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
SN : 0036004A3338510939303435
FW version : 0x0110
Device ID : 0x0500
Device name : STM32MPxxx
Device type : MPU
Device CPU : Cortex-A7
Start Embedded Flashing service
Memory Programming ...
Opening and parsing file: tf-a-stm32mp157c-dk2-trusted.stm32
File : tf-a-stm32mp157c-dk2-trusted.stm32
Size : 245360 Bytes
Partition ID : 0x01
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:04.627
RUNNING Program ...
PartID: :0x01
Start operation done successfully at partition 0x01
Flashlayout Programming ...
[==================================================] 100%
Running Flashlayout Partition ...
Flashlayout partition started successfully
Memory Programming ...
Opening and parsing file: u-boot-stm32mp157c-dk2-trusted.stm32
File : u-boot-stm32mp157c-dk2-trusted.stm32
Size : 748660 Bytes
Partition ID : 0x03
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:13.495
RUNNING Program ...
PartID: :0x03
reconnecting the device ...
Error: unable to reconnect the target device: time out expired
Error: Start operation failed at partition 0x03
Error: TSV flashing service failed
2019-07-25 12:29 AM
I changed the USB setting from "Full Speed" to "High Speed". It didn't help. It has the same problem.
2019-07-25 12:30 AM
but in Windows 10 with GUI CubeProgrammer it worked. in VM doesn't.
2019-07-25 1:04 AM
Good to see it is working on W10.
Please have a look to https://community.st.com/s/question/0D50X0000Az2Ct3SQE/how-do-i-load-openlinux-on-the-mp157
It is likely related to your VM behavior/settings around USB connection (e.g. in VMWare, you could check in 'removable device', if the 'STMicroelectronics USB download..." is connected to the VM and not to W10 host) .
2019-09-03 9:54 PM
I have exactly the same problem.
But it is solved when I add "-tm 20000".
2020-08-10 5:08 AM
I had similar issue as reported originally:
RUNNING Program ...
PartID: :0x03
reconnecting the device ...
For me the issue was solved by making sure that the VirtualBox guest has a USB-filter to re-claim the USB connection used. If this is not setup and the boot loader for some reason need to reconnect the device CubeProg in the VM guest will time out since it does not re-detect the USB-port of the MP1 device.
Did play with "-tm" option at all.
2023-02-06 4:10 PM
It's so annoying!
Equipment: Power supply 6A, native Ubuntu 22.04, USB Highspeed 480MBit/s
USB port disappears everytime and do you know what?
The board also, because I put it in the trash.
Tried many times to build a different linux image.
The only thing the board was good at: blinking a red LED, nice!