cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32mp157A SPI configuration At u boot level?

Sindhu Vadde
Associate III

Hi ,

We are using stm32mp157a processor in our custom board.We want to configure Spi1 to Ethernet Switch(ksz9893rnxia) (Note : we have 2 slaves for Spi1 at Uboot level(Source code ver 2018.11). I have done Pin control and node creations in dts files.

1) we are using spi_setup_slave(unsigned int bus, unsigned int cs,unsigned int max_hz, unsigned int mode) (In my case we gave parameters as follows spi_setup_slave(1,0,1000,0) for slave setup but We are getting 0 as return value.We confused about bus,cs,max_hz,mode parameters in spi_setup_slave() function.

path for spi_setup_slave Function :"https://elixir.bootlin.com/u-boot/v2018.11/source/drivers/spi/spi-uclass.c#L103".

2.if we have more than 1 slave how do we differentiate the cs numbers for spi.

3.which driver function is used for spi transmitting and receiving data.

Our spi related dts as follows.

board_level dts:

&spi1 {

       pinctrl-names = "default", "sleep";

       pinctrl-0 = <&spi1_pins_a>;

       pinctrl-1 = <&spi1_sleep_pins_a>;

       cs-gpios = <&gpioz 3 0>;

       status = "okay";

       ethernet-switch@0 {

               compatible = "microchip,KSZ9893RNXIA";

               reg = <0>; /* CS #0 */

               spi-max-frequency = <10000000>;

               #address-cells = <1>;

               #size-cells = <1>;

               spi-rx-bus-width = <8>;

               spi-tx-bus-width = <8>;

       };

};

Processor Related Dts:

 spi1_pins_a: spi1-0 {

                               pins1 {

                                       pinmux = <STM32_PINMUX('Z', 0, AF5)>, /* SPI1_SCK */

                                                <STM32_PINMUX('Z', 2, AF5)>, /* SPI1_MOSI */

                                       bias-disable;

                                       drive-push-pull;

                                       slew-rate = <1>;

                               };

                               pins2 {

                                       pinmux = <STM32_PINMUX('Z', 1, AF5)>; /* SPI1_MISO */

                                       bias-disable;

                               };

                       };

 spi1_sleep_pins_a: spi1-sleep-0 {

                               pins {

                                       pinmux = <STM32_PINMUX('Z', 0, ANALOG)>, /* SPI1_SCK */

                                                <STM32_PINMUX('Z', 1, ANALOG)>, /* SPI1_MISO */

                                                <STM32_PINMUX('Z', 2, ANALOG)>, /* SPI1_MOSI */

                               };

};

Is this correct way to configure spi?

Thanks in advance.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0