cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32mp157 optee ETC panic 0 0 ECO 5.0.3

MWoło.2
Senior III

Hello,

I encountered a problem with optee that I could not resolve due to a misunderstanding of debug information.

During boot up the board, I get the following debug log

Spoiler
...
F/TC:0 0 __clk_enable:1195 Clock 192 has been enabled
D/TC:0 0 probe_driver_node:550 element: stm32-rtc on node rtc@5c004000 initialized
F/TC:0 0 probe_driver_node:543 Probing stm32-iwdg on node watchdog@5a002000
F/TC:0 0 pager_deploy_page:1469 Mapped 0x30023000 -> 0x2fffa000
F/TC:0 0 pager_deploy_page:1469 Mapped 0x30056000 -> 0x2ffea000
F/TC:0 0 pager_deploy_page:1469 Mapped 0x30021000 -> 0x2fffd000
D/TC:0 0 gic_it_set_cpu_mask:410 cpu_mask: writing 0xff000000 to 0x349218b4
D/TC:0 0 gic_it_set_cpu_mask:412 cpu_mask: 0x3000000
D/TC:0 0 gic_it_set_prio:426 prio: writing 0x1 to 0x349214b7
D/TC:0 0 dt_driver_device_from_node_idx_prop:370 Property resets missing in node watchdog@5a002000
F/TC:0 0 __clk_enable:1195 Clock 58 has been enabled
D/TC:0 0 iwdg_wdt_get_version_and_status:528 Watchdog is enabled
F/TC:0 0 pager_deploy_page:1469 Mapped 0x30055000 -> 0x2ffed000
F/TC:0 0 pager_deploy_page:1469 Mapped 0x3001c000 -> 0x2fffb000
D/TC:0 0 register_periph_iomem:331 IO for non-secure resource 0x5a002000
E/TC:0 0 Panic

and with Panic at the end. I have to admit that I don't see any trouble with the debug text above.

I also attached two dts files tf-a and optee and full log. 

The files were generated from the latest STMCubeIde 1.17.0 with the necessary supplementation.

Thanks for any help

BR Michal

10 REPLIES 10
GatienC
ST Employee

Any chance this can be linked to:  problem-booting-optee-4-0-kernel-6-6 ?