2024-07-25 5:28 AM
I'm using minimal device tree files to get a custom (MYIR MYC-YF135) board to boot. At the moment I'm stuck when OP-TEE should give the control to u-boot. The boot stops on error message: No serial driver found
....
F/TC:0 0 _regulator_enable:150 vdd
F/TC:0 0 _regulator_enable:188 vdd refcount: 1
F/TC:0 0 _regulator_enable:150 v3v3
F/TC:0 0 _regulator_enable:188 v3v3 refcount: 1
F/TC:0 0 _regulator_enable:150 vddcore
F/TC:0 0 _regulator_enable:188 vddcore refcount: 1
F/TC:0 0 regulator_core_dump:920 Dump Regulators
F/TC:0 0 regulator_core_dump:921 reg name use en mV min max flags supply
F/TC:0 0 regulator_core_dump:941 usb33 usb33 0 0 3300 3300 3300 0
F/TC:0 0 regulator_core_dump:941 reg18 reg18 0 1 1800 1800 1800 0 vdd
F/TC:0 0 regulator_core_dump:941 reg11 reg11 0 1 1100 1100 1100 0 vdd
F/TC:0 0 iod_get_voltage:115 sdmmc1_io: get volt
F/TC:0 0 iod_get_state:104 sdmmc1_io: get state
F/TC:0 0 regulator_core_dump:941 sdmmc1_i sdmmc1_i 1 1 3300 0 65535 0x1 vdd
F/TC:0 0 iod_get_voltage:115 sdmmc2_io: get volt
F/TC:0 0 iod_get_state:104 sdmmc2_io: get state
F/TC:0 0 regulator_core_dump:941 sdmmc2_i sdmmc2_i 1 1 3300 0 65535 0x1 vdd
F/TC:0 0 regulator_core_dump:941 vdd vdd 1 1 3300 3300 3300 0x1
F/TC:0 0 regulator_core_dump:941 v3v3 v3v3 1 1 3300 3300 3300 0x1
F/TC:0 0 regulator_core_dump:941 vddcore vddcore 1 1 1350 1350 1350 0x1
D/TC:0 0 call_initcalls:40 level 6 scmi_regulator_consumer_init()
F/TC:0 0 get_supply_phandle:114 voltd: supplied by 7
D/TC:0 0 scmi_regulator_consumer_init:322 scmi voltd shares reg11 (node reg11) on domain ID 0
F/TC:0 0 get_supply_phandle:114 voltd: supplied by 8
D/TC:0 0 scmi_regulator_consumer_init:322 scmi voltd shares reg18 (node reg18) on domain ID 1
F/TC:0 0 get_supply_phandle:114 voltd: supplied by 9
D/TC:0 0 scmi_regulator_consumer_init:322 scmi voltd shares usb33 (node usb33) on domain ID 2
D/TC:0 0 call_initcalls:40 level 7 stm32_rng_release()
D/TC:0 0 call_initcalls:40 level 7 regulator_core_cleanup()
F/TC:0 0 regulator_core_cleanup:1008
D/TC:0 0 regulator_core_cleanup:1012 disable usb33
D/TC:0 0 regulator_core_cleanup:1012 disable reg18
D/TC:0 0 regulator_core_cleanup:1012 disable reg11
D/TC:0 0 call_initcalls:40 level 7 release_probe_lists()
D/TC:0 0 call_finalcalls:59 level 1 release_external_dt()
I/TC: Primary CPU switching to normal world boot
<debug_uart>
serial_stm32 serial@40010000: pinctrl_select_state_full: uclass_get_device_by_phandle_id: err=-19
serial_stm32 serial@40010000: pinctrl_select_state_full: uclass_get_device_by_phandle_id: err=-19
serial_stm32 serial@40010000: pinctrl_select_state_full: uclass_get_device_by_phandle_id: err=-19
serial_stm32 serial@40010000: pinctrl_select_state_full: uclass_get_device_by_phandle_id: err=-19
No serial driver found
resetting ...
System reset not supported on this platform
### ERROR ### Please RESET the board ###
mx-u-boot.dts
/ {
/* USER CODE BEGIN root */
aliases{
mmc0 = &sdmmc1;
};
config{
u-boot,mmc-env-partition = "u-boot-env";
};
/* USER CODE END root */
}; /*root*/
/* USER CODE BEGIN addons */
&uart4{
u-boot,dm-pre-reloc;
};
&uart4_pins_mx {
u-boot,dm-pre-reloc;
pins1 {
u-boot,dm-pre-reloc;
};
pins2 {
u-boot,dm-pre-reloc;
};
};
mx.dts
aliases{
serial0 = &uart4;
};
chosen{
stdout-path = "serial0:115200n8";
#address-cells = <1>;
#size-cells = <1>;
ranges;
framebuffer{
compatible = "simple-framebuffer";
clocks = <&rcc LTDC_PX>;
status = "disabled";
};
};
...
&uart4{
pinctrl-names = "default", "idle", "sleep";
pinctrl-0 = <&uart4_pins_mx>;
pinctrl-1 = <&uart4_idle_pins_mx>;
pinctrl-2 = <&uart4_sleep_pins_mx>;
status = "okay";
/* USER CODE BEGIN uart4 */
/delete-property/ dmas;
/delete-property/ dma-names;
/* USER CODE END uart4 */
};
I can't see anything related in optee.dts what should be enabled to get access to UART4 in u-boot. So what am I missing? Where could I start to look? And what is this error? Is it related to UART4? Well, at least it can print the last error messages to it.
2024-07-25 5:33 AM
Hi @jhi
this post might help you
Regards.
2024-07-25 5:39 AM
Yes I already saw it, but the base address (0x40010000) is correct for the UART4 (it is the default). And there are no switches in OP-TEE for UART4 as there are for USART2.
2024-07-25 5:51 AM
Here are my device tree files.
It is possible to attach only 3 files so the uboot-u-boot.dts is here:
// SPDX-License-Identifier: (GPL-2.0-or-later OR BSD-3-Clause)
/*
* Copyright (C) 2023, STMicroelectronics - All Rights Reserved
* Author: STM32CubeMX code generation for STMicroelectronics.
*/
/* For more information on Device Tree configuration, please refer to
* https://wiki.st.com/stm32mpu/wiki/Category:Device_tree_configuration
*/
/* USER CODE BEGIN includes */
#include "stm32mp13-u-boot.dtsi"
/* USER CODE END includes */
/ {
/* USER CODE BEGIN root */
aliases{
mmc0 = &sdmmc1;
};
config{
u-boot,mmc-env-partition = "u-boot-env";
};
/* USER CODE END root */
}; /*root*/
/* USER CODE BEGIN addons */
&uart4{
u-boot,dm-pre-reloc;
};
&uart4_pins_mx {
u-boot,dm-pre-reloc;
pins1 {
u-boot,dm-pre-reloc;
};
pins2 {
u-boot,dm-pre-reloc;
};
};
/* USER CODE END addons */
2024-07-29 6:20 AM
I have tried to debug this by adding print statements to serial-uclass.c.
In a function serial_check_stdout the chosen console is found serial0:115200n8, node 7780. Later the device uclass ID is UCLASS_SERIAL, but then the device_probe returns -ENODEV = No such device.
I did dump the tree of all devices
Class Index Probed Driver Name
-----------------------------------------------------------
root 0 [ + ] root_driver root_driver
simple_bus 0 [ ] simple_bus |-- soc
clk 0 [ ] fixed_clock |-- clk-mco1
serial 0 [ ] serial_stm32 `-- serial@40010000
So the serial is found.
uclass
uclass 95: serial
0 serial@40010000 @ c02803fc, seq 0
Driver
serial_stm32 095 serial serial@40010000
So any ideas why it still complains that it can't find the device?
2024-07-29 6:34 AM
I have forgotten to write, that I'm using the bootlin buildroot release st/2023.02.10
2024-07-30 7:13 AM
I went down the rabbit hole and managed to find, that the problem is clock, but I still don't know what is wrong:
Driver uid uclass Devices
----------------------------------------------------------
stm32mp13_clk 029 clk <none>
and uclass_foreach_dev(dev, uc) do not anything as us->(I don't know which one) is NULL and then the uclass_find_device_by_ofnode will return -ENODEV.
@PatrickF I would really appreciate a little help from your side. I don't know what the purpose of this community is, when you never get any answer. I still have few questions open and never got answer for those. I can also see, that there are lot of other questions from other users without any reaction from your side.
2025-02-05 12:38 PM
Hi Jhi,
I face similar issues, did you get the answer for it?