cancel
Showing results for 
Search instead for 
Did you mean: 

stm32mp135 PA10 as tim1 ch3 pwm

MWoło.2
Senior III

Hi,

I have a problem with the configuration of PA10 of stm32mp135 to work as pwm of TIM1_CH3. I also make an experiment to disable completely timer and PWM and I also can't control this pin using gpioset. In the documentation I saw that this pin is dedicated to USB "...OTG_HS_ID is on PA10 (EXTI10)". My question is simple how to disconnect PA10 from USB completely? CubeMx doesn't do that.

1 ACCEPTED SOLUTION

Accepted Solutions

I find a bit similar problem to my

https://community.st.com/t5/stm32-mpu-products/120-369992-dwc2-49000000-usb-otg-overcurrent-change-detected/td-p/168914

and finally, I created something like

&usbotg_hs{
	status = "okay";

	/* USER CODE BEGIN usbotg_hs */
	dr_mode = "peripheral";
	usb-role-switch;
	role-switch-default-mode = "peripheral"; 
	phys = <&usbphyc_port1 0>;
	phy-names = "usb2-phy";
	/* USER CODE END usbotg_hs */
};

 Now my gadget ethernet is working and backlight pwm also. Topic can be closed.

View solution in original post

7 REPLIES 7
MWoło.2
Senior III

I forgot to add that I try to do this on my custom board which has no physical connection with any USB lines.

MWoło.2
Senior III

The voltage on this PA10 pin is 3.17V, and my VDD is 3.3V.

Command

gpioset gpiochip0 '10'=0

don't change this value

this one

gpioset gpiochip0 '10'=1

also. This pin has to be somewhere configured to USB or another function.

In the system I have

MWoo2_0-1688118340848.png

 

PatrickF
ST Employee

Hi @MWoło.2 ,

Maybe have a look to "u-boot,force-b-session-valid" property in order to disable usage of ID pin.

https://wiki.st.com/stm32mpu/wiki/How_to_configure_U-Boot_for_your_board#USB_OTG_node

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
MWoło.2
Senior III

My usbotg_hs section has no 'u-boot,force-vbus-detection;'. I check it and give feedback. Thanks, BR Michal

Hi Patrick,

Unfortunately, additional record in the U-Boot DTS does not help. I discover something new. The 3.17V voltage on PA10 appears not in the U-Boot but after kernel start. So in my opinion the problem is not in the U-Boot but in the Kernel.

Records like 'force-vbus-detection' do not exist in any Kernel files.

How should look the Kernel DTS related to &usbotg_hs to disable the OTG_HS_ID function of PA10?

BR

Michal

MWoło.2
Senior III

I made a teenth of experiments with different parameters in the Kernel dts. The backlight PWM on PA10 works only in the configuration where the added parameter 'usb-role-switch'. Unfortunately in such a configuration gadget ethernet not working. I think it is impossible to set 'peripheral' without involving PA10.

So currently my kernel dts looks

&usbotg_hs{
	status = "okay";

	/* USER CODE BEGIN usbotg_hs */
	dr_mode = "usb-role-switch";
	usb-role-switch;
	phys = <&usbphyc_port1 0>;
	phy-names = "usb2-phy";
	/* USER CODE END usbotg_hs */
};

 I discover also that changing 'dr_mode = ...' to anything does nothing.

Finally, my question is, does it possible to set 'peripheral' and get PWM on PA10?

I find a bit similar problem to my

https://community.st.com/t5/stm32-mpu-products/120-369992-dwc2-49000000-usb-otg-overcurrent-change-detected/td-p/168914

and finally, I created something like

&usbotg_hs{
	status = "okay";

	/* USER CODE BEGIN usbotg_hs */
	dr_mode = "peripheral";
	usb-role-switch;
	role-switch-default-mode = "peripheral"; 
	phys = <&usbphyc_port1 0>;
	phy-names = "usb2-phy";
	/* USER CODE END usbotg_hs */
};

 Now my gadget ethernet is working and backlight pwm also. Topic can be closed.