2022-08-22 1:03 AM
Hello,
I would like to setup environment for STM32MPU according this instruction:
so I downloaded the SDK .tar
and run the script and got an error
./st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15.sh
Extracting SDK............................................................................................................................................................................................................................done
Setting it up...xargs: file: No such file or directory
sed: no input files
Failed to replace perl. Relocate script failed. Abort!
I run this script in docker based on ubuntu. All necessary packet installed.
FROM ubuntu:20.04
What could be a problem?
I run this script with -D (debug mode) and got:
I run this script in docker based on ubuntu. All necessary packet installed.
FROM ubuntu:20.04
What could be a problem?
I run this script with -D (debug mode) and got:
+ find /opt/st/stm32mp1/4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15 -maxdepth 1 -type f
+ xargs -n100 file
+ grep :.*\(ASCII\|script\|source\).*text
+ grep -Fv -e /opt/st/stm32mp1/4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/environment-setup- -e /opt/st/stm32mp1/4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/relocate_sdk -e /opt/st/stm32mp1/4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/post-relocate-setup -e /opt/st/stm32mp1/4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15.sh
+ xargs -n100 sed -i -e s:/usr/local/oe-sdk-hardcoded-buildpath:/opt/st/stm32mp1/4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15:g -e s:^#! */usr/bin/perl.*:#! /usr/bin/env perl:g -e s: /usr/bin/perl: /usr/bin/env perl:g
+ awk -F: {printf "\"%s\"\n", $1}
+ find /opt/st/stm32mp1/4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/sysroots/x86_64-ostl_sdk-linux -type f
xargs: file: No such file or directory
sed: no input files
+ [ 123 -ne 0 ]
+ echo Failed to replace perl. Relocate script failed. Abort!
Failed to replace perl. Relocate script failed. Abort!
Solved! Go to Solution.
2022-09-20 7:07 AM
Hello,
Yes,
The solution is here:
I must have created duplication and did not remove one of it. Sorry for that.
2022-09-09 5:03 AM
Hello,
I would recommend to try again..
I just tried from scratch according the web page you mentioned.
I am using Ubuntu 20.04 64bit
I have the below commands:
$ sudo apt-get update
$ sudo apt-get install gawk wget git diffstat unzip texinfo gcc build-essential chrpath socat cpio python3 python3-pip python3-pexpect xz-utils debianutils iputils-ping python3-git python3- libegl1-mesa libsdl1.2-dev pylint3 xterm python3-subunit mesa-common-dev zstd liblz4-tool
$ sudo apt-get install make xsltproc docbook-utils fop dblatex xmlto
$ sudo apt-get install libmpc-dev libgmp-dev
$ sudo apt-get install build-essential libncurses-dev libyaml-dev libssl-dev
$ sudo apt install python-is-python3
$ sudo apt-get install coreutils bsdmainutils sed curl bc lrzsz corkscrew cvs subversion mercurial nfs-common nfs-kernel-server libarchive-zip-perl dos2unix texi2html diffstat libxml2-utils
$ echo 'options mmc_block perdev_minors=16' > /tmp/mmc_block.conf
$ sudo mv /tmp/mmc_block.conf /etc/modprobe.d/mmc_block.conf
$ mkdir -p $HOME/STM32MPU_workspace/STM32MP1-Ecosystem-v4.0.0/Developer-Package/SDK
$ cd /home/osboxes/STM32MPU_workspace
$ mkdir tmp
$ “move downloaded and unziped SDK folder in tmp�?
$ cd tmp/en.SDK-x86_64-stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/sdk/
$ chmod +x st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15.sh
$ cd ../../
$ ./stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/sdk/st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15.sh
ST OpenSTLinux - Weston - (A Yocto Project Based Distro) SDK installer version 4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15
===================================================================================================================================
Enter target directory for SDK (default: /opt/st/stm32mp1/4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15):
You are about to install the SDK to "/opt/st/stm32mp1/4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15". Proceed [Y/n]?
Extracting SDK............................................................................................................................................................................................................................done
Setting it up...done
SDK has been successfully set up and is ready to be used.
Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g.
$ . /opt/st/stm32mp1/4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
JM
2022-09-19 11:36 AM
Hello @ZHala.1 ,
Have you been able to fix this issue?
Regards,
Kevin
2022-09-20 7:07 AM
Hello,
Yes,
The solution is here:
I must have created duplication and did not remove one of it. Sorry for that.
2022-09-20 8:50 AM
Hello @ZHala.1 ,
Oh ok it was me that answered :D. I didn't see that your name was the same.
Best Regards,
Kevin
2023-08-14 1:57 AM
Hi,
@Kevin HUBER what was the solution to this issue?
I'm seeing the same issue (docker image ubuntu:22.04), the link posted by @ZHala.1 is unfortunately dead ("An invalid set of parameters has been specified in the url.").
Bests,
amuew
2023-08-18 6:34 AM
Hello @amuew ,
Sorry for that, I will ask to fix this link.
It's been a long time, so I'm not sure, but I think this was this post: https://community.st.com/t5/stm32-mpu-products/sdk-installation-script/td-p/123436
Best Regards,
Kevin