2023-02-27 11:07 AM
I have several devices connected through a CAN network. Using an STM32MP1 I want to build a web frontend that can be used to not only issue commands but also receive arbitrary data and present it to the user. (Data from the devices).
I'm trying to figure out what applications/stack that I should use for this? I don't mind customizing, but would prefer to use something that I can build on to. My CAN network code is already written (ported from other STM32 HAL projects). So I can use that as a standalone piece of software and integrate it through sockets, or similar.