cancel
Showing results for 
Search instead for 
Did you mean: 

receipt.bb can't install into /usr/local in latest V4.0.x OpenSTLinux

MWoło.2
Senior III

Hi,

I have a problem with installing any directory or any files into /usr/local folder.

Here my_receipt.bb

DESCRIPTION = "My receipt"
LICENSE = "BSD-3-Clause"
LIC_FILES_CHKSUM = "file://${COREBASE}/meta/files/common-licenses/BSD-3-Clause;md5=550794465ba0ec5312d6919e203a55f9"
 
SRC_URI = "file://reset_led.sh "
 
S = "${WORKDIR}"
 
do_configure[noexec] = "1"
do_compile[noexec] = "1"
 
do_install() {
    install -d ${D}${prefix}/local/reset-led
    install -m 0755 ${WORKDIR}/reset_led.sh ${D}${prefix}/local/reset-led/
}
 
FILES:${PN} += "${prefix}/local/reset-led/"

In OpenSTLinx, those folders and files go to st-image-userfs...tar.xz.

In /usr/local I can see only demos etc. folders and directories.

The compilation is going well without any errors or warnings. What was missed, and where is the problem?

1 ACCEPTED SOLUTION

Accepted Solutions
Erwan SZYMANSKI
ST Employee

Hi @Michał Wołowik​ ,

Yes understood, indeed this is a userfs mounting point issue.

What is happening here is that you tell the weston image to install your package in /usr/local.

However, we also have a userfs image that aims to install everything in this folder, so a complete clean is made before.

What you have to do is to tell this userfs image to install your package.

It is done in the following file: layers/meta-st/meta-st-stm32mp/recipes-st/images/st-image-userfs.bb

Then, modify the file to add your "my-receipt" package.

SUMMARY = "STM32MP userfs Image"
LICENSE = "MIT"
 
include recipes-st/images/st-image-partitions.inc
 
# Define to null ROOTFS_MAXSIZE
IMAGE_ROOTFS_MAXSIZE = ""
 
# Add specific package for our image:
PACKAGE_INSTALL += " \
    ${@bb.utils.contains('MACHINE_FEATURES', 'm4copro', 'm4projects-stm32mp1-userfs', '', d)} \
    linux-examples-stm32mp1-userfs \
    my_receipt \
    "
 
# Add demo application described on specific packagegroup
PACKAGE_INSTALL += " \
    packagegroup-st-demo \
    "

Hope that it will help you.

Kind regards,

Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

6 REPLIES 6
Erwan SZYMANSKI
ST Employee

Hello @Michał Wołowik​ ,

Did you already compare with the /layers/meta-st/meta-st-stm32mp/recipes-extended/linux-examples/linux-examples-stm32mp1 bitbake file ?

Let me know if you understand your issue with the upper file that do the same thing as what you are looking for.

For now I am building a yocto image with your example to try to reproduce.

Kind regards,

Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
MWoło.2
Senior III

Hi Erwan,

yes, I based on linux-examples-stm32mp1. The problem is that no folder reset-led is created into /usr/local. I also try to add a folder in for instance into /etc/systemd/system and working as it should. The problem is only with /usr/local. I predict a problem with userfs partition due it is the mounting point for /usr/local.

Thanks for the help.

BR Michal

Erwan SZYMANSKI
ST Employee

Hi @Michał Wołowik​ ,

Yes understood, indeed this is a userfs mounting point issue.

What is happening here is that you tell the weston image to install your package in /usr/local.

However, we also have a userfs image that aims to install everything in this folder, so a complete clean is made before.

What you have to do is to tell this userfs image to install your package.

It is done in the following file: layers/meta-st/meta-st-stm32mp/recipes-st/images/st-image-userfs.bb

Then, modify the file to add your "my-receipt" package.

SUMMARY = "STM32MP userfs Image"
LICENSE = "MIT"
 
include recipes-st/images/st-image-partitions.inc
 
# Define to null ROOTFS_MAXSIZE
IMAGE_ROOTFS_MAXSIZE = ""
 
# Add specific package for our image:
PACKAGE_INSTALL += " \
    ${@bb.utils.contains('MACHINE_FEATURES', 'm4copro', 'm4projects-stm32mp1-userfs', '', d)} \
    linux-examples-stm32mp1-userfs \
    my_receipt \
    "
 
# Add demo application described on specific packagegroup
PACKAGE_INSTALL += " \
    packagegroup-st-demo \
    "

Hope that it will help you.

Kind regards,

Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
MWoło.2
Senior III

Hi Erwan,

I will try.

Thanks

BR Michal

MWoło.2
Senior III

Perfect answer. It is always good to ask, I spend almost half a day. Of course works. Many thanks

BR Michal

@Michał Wołowik​ ,

Glad to see that it solves your issue.

Have a nice day,

Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.