Skip to main content
Associate III
May 15, 2024
Solved

"EQOS_DMA_MODE_SWR stuck FAILED: -110" error for ethernet in uboot

  • May 15, 2024
  • 6 replies
  • 3103 views

Hi everyone,

recently we have developed a custom board based on stm32mp157 mpu. We have used openstlinux distribution and the branch is "kirkstone". Ethernet is working perfectly on the Linux kernel. But problem arises when I am in the uboot mode (We want to have access to the ethernet from uboot). First, the ethernet can not find the mac address. It shows the following Error:

 

 

invalid MAC address 0 in OTP 00:00:00:00:00:00

Error: ethernet@5800a000 address not set.
No ethernet found.

 

 
The I set the ethernet mac address using the "setenv" command and then I enter dhcp command to test the ethernet connection, it shows the following error:
 

 

EQOS_DMA_MODE_SWR stuck FAILED: -110 in stm32mp157 for u-boot

 

 

I have the following configuration for the ethernet in uboot device tree.

 

 

&ethernet0{
 pinctrl-names = "default", "sleep";
 pinctrl-0 = <&eth1_pins_mx>;
 pinctrl-1 = <&eth1_sleep_pins_mx>;
 status ="okay";

 /* USER CODE BEGIN ethernet0 */
 phy-mode = "rmii";
 max-speed = <100>;
 phy-handle = <&phy0>;
 phy-supply = <&vdd_usb>;
 nvmem-cells = <&ethernet_mac_address>;
 nvmem-cell-names = "mac-address";

 clock-names = "stmmaceth",
 "mac-clk-tx",
 "mac-clk-rx",
 "ethstp",
 "eth-ck",
 "syscfg-clk";
 clocks = <&rcc ETHMAC>,
 <&rcc ETHTX>,
 <&rcc ETHRX>,
 <&rcc ETHSTP>,
 <&rcc ETHCK_K>,
 <&rcc SYSCFG>;
 st,eth_ref_clk_sel;
 phy-reset-gpios = <&gpiob 0 GPIO_ACTIVE_LOW>;

 mdio0 {
 #address-cells = <1>;
 #size-cells = <0>;
 compatible = "snps,dwmac-mdio";
 phy0: ethernet-phy@0 {
 reset-gpios = <&gpiob 0 GPIO_ACTIVE_LOW>;
 reset-duration = <200>;
 reg = <0>;
 };
 };
 /* USER CODE END ethernet0 */
};

 

 

Can anyone help me to solve those above two errors? Thanks in advance.

This topic has been closed for replies.
Best answer by ahamod3.1416

Finally got the solution for the Error. This Error basically indicate the clock issue. EQOS_DMA_MODE_SWR function is being called if software reset is not done in the SWR time interval. I set the wrong clock. I figured it out by measuring the clock using oscilloscope.

6 replies

Associate III
May 17, 2024

I got solution for the the first problem in defconfig I added "CONFIG_NET_RANDOM_ETHADDR=y".

Which is getting a random mac address. Now I do not have to set the mac address manually. But still I have the second error and can not establish the connection with the internet.

ahamod3.1416AuthorBest answer
Associate III
May 24, 2024

Finally got the solution for the Error. This Error basically indicate the clock issue. EQOS_DMA_MODE_SWR function is being called if software reset is not done in the SWR time interval. I set the wrong clock. I figured it out by measuring the clock using oscilloscope.

TBind.2
Associate
December 17, 2024

Hello, do you recall how you fixed this issue. Which clock is incorrect? Can you maybe show the dt after the fix?

Associate III
December 21, 2024

Hi TBind.2, first of all sorry for late reply, as I am in vacation. In u-boot 2021, ethernet node you have to change the clock name, instead of 

st,eth_ref_clk_sel

 

use the following clock, 

st,ext-phyclk;

 

This change solved my issue.