cancel
Showing results for 
Search instead for 
Did you mean: 

Questions Regarding QuadSPI in STM32MP13 Bare Metal

SL1
Associate III

Currently, I am testing QuadSPI.

Is it correct for the output to include Command / Address / Data?

I want to output only Data. While I can remove the Address through settings, I couldn't remove the Command.

Is it possible to output only Data?

2 REPLIES 2
PatrickF
ST Employee

Hi @SL1 

QUADSPI is build to interface external Flash or similar.

For you concern, did you try playing with IMODE setting ?

PatrickF_0-1718895899603.png

Regards

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi, I recently solved this problem.

After checking, it was due to the ClockMode in the code below.

When I changed that part to XSPI_CLOCK_MODE_0, it worked correctly.

Is it correct that if it is set to XSPI_CLOCK_MODE_3, the address should be output before the data is output?

I will finish the post after confirming the answer.