cancel
Showing results for 
Search instead for 
Did you mean: 

Questions about burning erroI found the following errors when I burned kernel alone and starterpackage. May I ask why this was caused? The kernel is through https://github.com/STMicroelectronics/meta-st-stm32mp/blob/dunfell/recipes-kernel/linux/linux-strs

Ffu.1
Associate II

I found the following errors when I burned kernel alone and starterpackage. May I ask why this was caused? The kernel is through https://github.com/STMicroelectronics/meta-st-stm32mp/blob/dunfell/recipes-kernel/linux/linux-stm32mp/README.HO W_to.txt teaching burn, Starterpackage is delivered via STM32_Programmer_CLI -c port= USb1 -w Flashlayout_st - image - weston/trusted/FlashLayout_sdcard_stm32mp157c - dk2 - trusted. TSV

11 REPLIES 11

I find that sometimes it can be successfully burned and sometimes it is not successful. I don't know if it is the board problem. I don't know if you want to

Olivier GALLIEN
ST Employee

Hi @Ffu.1​ ,

What is your SDcard reference also ? Can you try another one ?

Seems you flash from Linux station ? Which OS ?

Thanks

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.