cancel
Showing results for 
Search instead for 
Did you mean: 

problems with installing fftw package

VKare.1
Associate II

Hi! Have some problems with installing fftw package. I tried to install it to st-image-weston and st-example-image-xfce, but received same error when bitbake run do_rootfs. Can anybody explain this problem?

Build Configuration:

BB_VERSION          = "1.40.0"

BUILD_SYS           = "x86_64-linux"

NATIVELSBSTRING     = "universal"

TARGET_SYS          = "arm-openstlinux_x11-linux-gnueabi"

MACHINE             = "stm32mp1"

DISTRO              = "openstlinux-x11"

DISTRO_VERSION      = "2.6-snapshot-20191213"

TUNE_FEATURES       = "arm armv7ve vfp thumb neon vfpv4 callconvention-hard cortexa7"

TARGET_FPU          = "hard"

DISTRO_CODENAME     = "thud"

ACCEPT_EULA_stm32mp1 = "1"

GCCVERSION          = "8.%"

PREFERRED_PROVIDER_virtual/kernel = "linux-stm32mp"

meta-python          

meta-oe              

meta-oe              

meta-gnome           

meta-xfce            

meta-initramfs       

meta-multimedia      

meta-networking      

meta-webserver       

meta-filesystems     

meta-perl            

meta-python         

meta-st-stm32mp      

meta-qt5             

meta-st-openstlinux  

meta                = "master:364b6270b0787afe634252406c4c559ba592b6a3"

workspace           = "<unknown>:<unknown>"

meta-qt4            = "master:ec8e0800ef1c33b72f3d3924412dabc48c2a55ac"

Initialising tasks: 100% |###########################################################################################################################################################################| Time: 0:00:13

Sstate summary: Wanted 448 Found 442 Missed 6 Current 3139 (98% match, 99% complete)

NOTE: Executing SetScene Tasks

NOTE: Executing RunQueue Tasks

ERROR: st-image-powmach-1.0-r0 do_rootfs: Unable to install packages. Command '/home/vlad/STM32MPU_workspace/STM32MP15-Ecosystem-v1.1.0/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/build-openstlinuxx11-stm32mp1/tmp-glibc/work/stm32mp1-openstlinux_x11-linux-gnueabi/st-image-powmach/1.0-r0/recipe-sysroot-native/usr/bin/apt-get install --force-yes --allow-unauthenticated apt dpkg packagegroup-base-extended packagegroup-core-boot packagegroup-core-eclipse-debug packagegroup-core-ssh-dropbear packagegroup-core-tools-profile packagegroup-core-x11 packagegroup-framework-core packagegroup-framework-core-base packagegroup-framework-sample-xfce packagegroup-framework-tools packagegroup-framework-tools-base psplash-drm resize-helper run-postinsts systemd-mount-partitions xf86-video-modesetting' returned 100:

Reading package lists...

Building dependency tree...

Reading state information...

Some packages could not be installed. This may mean that you have

requested an impossible situation or if you are using the unstable

distribution that some required packages have not yet been created

or been moved out of Incoming.

The following information may help to resolve the situation:

The following packages have unmet dependencies:

packagegroup-framework-sample-xfce : Depends: fftw but it is not installable

E: Unable to correct problems, you have held broken packages.

ERROR: st-image-powmach-1.0-r0 do_rootfs: Function failed: do_rootfs

ERROR: Logfile of failure stored in: /home/vlad/STM32MPU_workspace/STM32MP15-Ecosystem-v1.1.0/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/build-openstlinuxx11-stm32mp1/tmp-glibc/work/stm32mp1-openstlinux_x11-linux-gnueabi/st-image-powmach/1.0-r0/temp/log.do_rootfs.28752

ERROR: Task (/home/vlad/STM32MPU_workspace/STM32MP15-Ecosystem-v1.1.0/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/layers/meta-st/meta-st-openstlinux/recipes-st/images/st-image-powmach.bb:do_rootfs) failed with exit code '1'

1 ACCEPTED SOLUTION

Accepted Solutions
KnarfB
Principal III

How did you try to add this package to the image? There is a subtle difference between recipe names and package names. The fftw recipe can build a package named libfftw, see fftw_3.3.6.bb. Try to add libfftw to your image.

hth

KnarfB

View solution in original post

1 REPLY 1
KnarfB
Principal III

How did you try to add this package to the image? There is a subtle difference between recipe names and package names. The fftw recipe can build a package named libfftw, see fftw_3.3.6.bb. Try to add libfftw to your image.

hth

KnarfB