2021-02-10 10:55 AM
I am working on the STM32MP157A. Setting PLL in the STM32CubeIDE does not work as expected. 24 MHz HSE DIVM4 = /5 DIVN4 = X84 DIVQ4 = /5 should = 80,460,000 . The MX program says 80,960,039. I do not understand.
If the MX program is right, then what is the equation?
I am trying to find the right combination to exactly get 460800 baud to work. The numbers I used should have worked.
Solved! Go to Solution.
2021-02-11 12:53 AM
Hi,
You probably have non-zero value in fracv4 field. I get 80,960,039 with frav4=2731.
Btw, there is probably a typo as with the values you provided you will get 80,640,000 (and not 80,460,000) with fracv4=0.
Could you please confirm the CubeIDE version you are using.
Regards.
2021-02-11 12:53 AM
Hi,
You probably have non-zero value in fracv4 field. I get 80,960,039 with frav4=2731.
Btw, there is probably a typo as with the values you provided you will get 80,640,000 (and not 80,460,000) with fracv4=0.
Could you please confirm the CubeIDE version you are using.
Regards.
2021-02-11 7:42 AM
My typing leads much to be desired. Yes I get 80,640,000
I am using :
Version: 1.5.1
Build: 9029_20201210_1234 (UTC)
I just redid it and you were right. fracv4 was not zero. I did not even notice it. It is zero and I get 80.64 MHz as expected.
Thank you,
Kip