2024-02-21 9:45 PM
Hi All.
I use discovery board of STM32MP157F-DK2 .
So I want t to try read OTP Bits via STM32CubeProgrammer , But I find 2 errs.
The err things search ST Community, I fund it.
Can't read OTP bits on STM32MP157C-DK2 using STM32CubeProgrammer
So I Try to refer Answer,I can't know where wrong.
(I reload Flashlayout for OTP exposing )
Sorry for my poor English,Thinks at all.
/********************************************************************************************************************/
u6326@Prodisk:~/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin$ ./STM32_Programmer_CLI -c port=usb1 -d FlashLayout.tsv -otp displ
-------------------------------------------------------------------
STM32CubeProgrammer v2.15.0
-------------------------------------------------------------------
USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2001, @Name /STM32MP157FAC Rev.Z,
SN : 003200433132511831373339
DFU protocol: 1.1
Board : --
Device ID : 0x0500
Device name : STM32MP157FAC Rev.Z
Device type : MPU
Revision ID : --
Device CPU : Cortex-A7
Start Embedded Flashing service
Flashing service completed successfully
UPLOADING OTP STRUCTURE ...
Partition : 0xF2
Size : 1024 Bytes
Uploading OTP data:
Error: Read OTP Partition failed
Error: Uploading the OTP structure failed
Error: Initializing the OTP structure failed
/********************************************************************************************************************/
Solved! Go to Solution.
2024-04-09 1:55 PM
Hello @thomas_sato ,
Sorry for the delay to answer, but I think we already answered your question in an internal ticket.
I explain here why you were not able to dump the OTP because it may help other people.
As explained in your previous post, you are using: Distribution-package in openstlinux-6.1-yocto-mickledore mickledoremp1-v23.11.15
That is the OSTL v5.0.2.
If you are using an OSTL v5.0.0 or newer you have to take care to the warning area of the wiki page: https://wiki.st.com/stm32mpu/wiki/OP-TEE_OTP_overview#OP-TEE_OS_configuration
You have to enable "CFG_WITH_USER_TA=y" to be able to read the OTP.
Hope it helps,
Best Regards,
Kevin
2024-02-22 2:43 AM
Hi @thomas_sato
Could it be same reason as in Solved: Can't read OTP bits on STM32MP157C-DK2 using STM32... - STMicroelectronics Community ?
Olivier
2024-02-22 5:11 PM
Hi.IlivierG.
think you for your cooperation.
Yes,I read and try it community page,But I can't do it.
Host OS is ubuntu 22.04,I check DFU driver is functional,Okey...
Am I generate failed file [ tf-a-stm32mp157f-dk2-usb.stm32 ] or [ fip-stm32mp157f-dk2-optee.bin ]?
I use Distributin-package in openstlinux-6.1-yocto-mickledore mickledoremp1-v23.11.15.
So I will set [ DISTRO=openstlinux-weston MACHINE=stm32mp1 source layers/meta-st/scripts/envsetup.sh ]
and [ bitbake se-image-weston ].
Can I Need special method for OTP paramer?
Best regards
2024-04-09 1:55 PM
Hello @thomas_sato ,
Sorry for the delay to answer, but I think we already answered your question in an internal ticket.
I explain here why you were not able to dump the OTP because it may help other people.
As explained in your previous post, you are using: Distribution-package in openstlinux-6.1-yocto-mickledore mickledoremp1-v23.11.15
That is the OSTL v5.0.2.
If you are using an OSTL v5.0.0 or newer you have to take care to the warning area of the wiki page: https://wiki.st.com/stm32mpu/wiki/OP-TEE_OTP_overview#OP-TEE_OS_configuration
You have to enable "CFG_WITH_USER_TA=y" to be able to read the OTP.
Hope it helps,
Best Regards,
Kevin
2024-04-10 10:26 PM
Thinks a lot !