2023-08-21 1:56 PM - edited 2023-08-21 1:58 PM
I am trying to migrate from ecosystem 4.1.0 to 5.0.0 however after getting all the device trees to compile and build plus a new image I am encountering a Panic in optee. The problem is that it just says Panic and I can't tell based on the debug prints which direction to take.
The board is a custom design based on the stm32mp157a-dk1 and all the vital components are the same (PMIC, SDMMC, etc)
Any suggestions on how I could debug this further?
I have attached the full debug console logs and is what I get from the console without the optee debug prints since it's too many lines:
�NOTICE: CPU: STM32MP153AAC Rev.Z
NOTICE: Model: STMicroelectronics custom STM32CubeMX board - openstlinux-6.1-yocto-mickledore-mp1-v23.06.21
NOTICE: Board: MBfdd8 Var2.15 Rev.B-14
INFO: Reset reason (0x15):
INFO: Power-on Reset (rst_por)
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe2000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using SDMMC
INFO: Instance 1
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.8-stm32mp1-r1.0(release):2023.05.1(7814dbce)
NOTICE: BL2: Built : 16:28:56, Aug 21 2023
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000kHz
INFO: Memory size = 0x10000000 (256 MB)
INFO: BL2: Loading image id 1
INFO: Loading image id=1 at address 0x2ffff000
INFO: Image id=1 loaded: 0x2ffff000 - 0x2ffff1ea
INFO: FCONF: Reading FW_CONFIG firmware configuration file from: 0x2ffff000
INFO: FCONF: Reading firmware configuration information for: dyn_cfg
INFO: FCONF: Reading firmware configuration information for: stm32mp1_firewall
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0x2ffc0000
INFO: Image id=4 loaded: 0x2ffc0000 - 0x2ffc002c
INFO: OPTEE ep=0x2ffc0000
INFO: OPTEE header info:
INFO: magic=0x4554504f
INFO: version=0x2
INFO: arch=0x0
INFO: flags=0x0
INFO: nb_images=0x2
INFO: BL2: Loading image id 8
INFO: Loading image id=8 at address 0x2ffc0000
INFO: Image id=8 loaded: 0x2ffc0000 - 0x2ffd38c0
INFO: BL2: Loading image id 9
INFO: Loading image id=9 at address 0xce000000
INFO: Image id=9 loaded: 0xce000000 - 0xce05c000
INFO: BL2: Loading image id 2
INFO: Loading image id=2 at address 0xc0500000
INFO: Image id=2 loaded: 0xc0500000 - 0xc0513ed8
INFO: BL2: Skip loading image id 16
INFO: BL2: Loading image id 5
INFO: Loading image id=5 at address 0xc0100000
INFO: Image id=5 loaded: 0xc0100000 - 0xc01f5d7c
NOTICE: BL2: Booting BL32
INFO: Entry point address = 0x2ffc0000
INFO: SPSR = 0x1d3
I/TC: Early console on UART#4
I/TC:
I/TC: Pager is enabled. Hashes: 3040 bytes
I/TC: Pager pool size: 92kB
I/TC: Embedded DTB found
I/TC: OP-TEE version: 2023.05.1 (gcc version 10.3.1 20210621 (GNU Toolchain for the A-profile Architecture 10.3-2021.07 (arm-10.29))) #1 Mon Aug 21 20:28:44 UTC 2023 arm
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html
I/TC: Primary CPU initializing
E/TC:0 0 Panic
Solved! Go to Solution.
2023-10-27 6:24 AM
@Kevin HUBERthe issue had nothing to do with the toolchain but with the fact that RNG1 was not assigned to the secure core in CubeMX.
2023-09-04 5:26 AM
Hello @cfilipescu ,
I can see in your log:
I/TC: OP-TEE version: 2023.05.1 (gcc version 10.3.1 20210621 (GNU Toolchain for the A-profile Architecture 10.3-2021.07 (arm-10.29))) #1 Mon Aug 21 20:28:44 UTC 2023 arm
I don't understand how you were able to have an optee for V5.0.0 built with "gcc version 10.3.1".
If you have a look at the default log that you should have on v5.0.0, you can see that the "gcc version 12.2.0" is normally the one used to generate the image:
I/TC: OP-TEE version: 3.19.0-dev (gcc version 12.2.0 (GCC)) #1 Fri Oct 14 19:00:05 UTC 2022 arm
In your case it looks like you built the OP-TEE image with a SDK from a previous Ecosystem.
Please can you start again to download the SDK of the DV5.0.0 in the getting started:
https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2/Develop_on_Arm%C2%AE_Cortex%C2%AE-A7/Install_the_SDK
And be sure to start it before building the OP-TEE:
If you want to follow the getting started from the beginning, you can start here: https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2/Let%27s_start/Populate_the_target_and_boot_the_image
Best Regards,
Kevin
2023-10-27 6:24 AM
@Kevin HUBERthe issue had nothing to do with the toolchain but with the fact that RNG1 was not assigned to the secure core in CubeMX.