2019-11-14 3:56 AM
Hi, I try to add a new layer and a new machine to the STM32MP1 Distribution Image. i followed the following tutorials tutorials:
https://wiki.st.com/stm32mpu/wiki/How_to_create_a_new_open_embedded_layer
https://wiki.st.com/stm32mpu/wiki/How_to_compile_the_device_tree_with_the_Distribution_Package
However, I am still getting the following error:
WARNING: st-image-core-1.0-r0 do_populate_lic: Could not copy license file /home/user/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/layers/meta-st/meta-st-stm32mp-addons/conf/eula/stm32mp1-mymachine to /home/user/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/build-openstlinuxeglfs-stm32mp1-mymachine/tmp-glibc/work/stm32mp1_mymachine-openstlinux_eglfs-linux-gnueabi/st-image-core/1.0-r0/license-destdir/st-image-core/stm32mp1-mymachine: [Errno 2] No such file or directory: '/home/user/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/layers/meta-st/meta-st-stm32mp-addons/conf/eula/stm32mp1-mymachine'
ERROR: st-image-core-1.0-r0 do_populate_lic: QA Issue: st-image-core: LIC_FILES_CHKSUM points to an invalid file: /home/user/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/layers/meta-st/meta-st-stm32mp-addons/conf/eula/stm32mp1-mymachine [license-checksum]
ERROR: st-image-core-1.0-r0 do_populate_lic: Fatal QA errors found, failing task.
ERROR: st-image-core-1.0-r0 do_populate_lic: Function failed: populate_lic_qa_checksum
ERROR: Logfile of failure stored in: /home/user/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/build-openstlinuxeglfs-stm32mp1-mymachine/tmp-glibc/work/stm32mp1_mymachine-openstlinux_eglfs-linux-gnueabi/st-image-core/1.0-r0/temp/log.do_populate_lic.30716
ERROR: Task (/home/user/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/layers/meta-st/meta-st-openstlinux/recipes-st/images/st-image-core.bb:do_populate_lic) failed with exit code '1'
So it looks that the bibtake still looks for the license file in the meta-st-stm32mp-addons, but not in my layer directory. Is there something I need to add to the configuration described in the tutorials from stm32mp1 wiki? I have already created the conf/eula directory in my layer with the link stm32mp1-mymachine -> ST_EULA_SLA.
Best regards,
Krzysztof
Solved! Go to Solution.
2019-12-04 8:26 AM
Pay attention to put MACHINEOVERRIDES .= ":stm32mpmydemo" at the end of your conf file.
It might be the last one in the MACHINEOVERRIDES list.
Olivier
2019-11-19 4:40 AM
Hi @Community member
Reading this page :
https://wiki.st.com/stm32mpu/wiki/How_to_create_your_own_machine
Did you do the symbolic link as described in Chapter 3.3 ?
Error message looks obvious that stm32mp1-mymachine -> ST_EULA_SLA. is missing in <path of STM32MP1_Distribution_Package>/layers/meta-st/meta-st-stm32mp-addons/conf/eula
Hope it help
Olivier
2019-11-19 4:57 AM
Hi Olivier,
thanks for the response. I have also tried the intrustions in the mentioned link, but without any success. If I create the symbolic link with my machine name in the meta-st-stm32mp-addons layer it works, however when I put it in the eula directory in my own layer and create the license symbolic link there I get the No such file or directory error. I have also added the layers/meta-st/meta-st-stm32mp-addons layer as needed bsp in my machine conf file (NEEDED_BSPLAYERS).
So it looks like my layer path is not searched for the license. I probably missed something to add it to the path but cannot find what.
Krzysztof
2019-11-28 2:26 AM
Hi @Community member
Did you still have the issue ?
If yes can you please share your layer.conf ?
Thx
Olivier
2019-12-03 3:28 AM
Hi Olivier,
Yes - the problem still exists. i tried a few more changes in the layer and machine configs but without success.
My layer.conf file looks like this:
# We have a conf and classes directory, add to BBPATH
BBPATH .= ":${LAYERDIR}"
# We have recipes-* directories, add to BBFILES
BBFILES += "${LAYERDIR}/recipes-*/*/*.bb \
${LAYERDIR}/recipes-*/*/*.bbappend"
BBFILE_COLLECTIONS += "meta-mylayer"
BBFILE_PATTERN_meta-mylayer = "^${LAYERDIR}/"
BBFILE_PRIORITY_meta-mylayer = "7"
# Set a variable to get the STM32MP MX BSP location
STM32MP_MYLAYER_BASE = "${LAYERDIR}"
# This should only be incremented on significant changes that may
# cause compatibility issues with other layers
LAYERVERSION_meta-mylayer = "1"
LAYERSERIES_COMPAT_meta-mylayer = "thud"
LAYERDEPENDS_meta-mylayer = "stm-st-stm32mp-mx"
2019-12-04 12:53 AM
Hi @Community member
Did you follow wiki page https://wiki.st.com/stm32mpu/wiki/How_to_compile_the_device_tree_with_the_Distribution_Package ?
Seems that your layer.conf does not contain lines related to EULA :
EULA_FILE_ST_stm32mpmylayer = "${LAYERDIR}/conf/eula/${MACHINE}"
EULA_FILE_ST_MD5SUM_stm32mpmylayer = "8b505090fb679839cefbcc784afe8ce9"
#Inform bitbake for adding another location to search for licenses
LICENSE_PATH += "${LAYERDIR}/files/licenses"
And in your machine .conf add :
MACHINEOVERRIDES .= ":stm32mpmylayer"
Hope it help
Olivier
2019-12-04 3:54 AM
Hi Olivier,
I'm sorry - I sent you the version of layer.conf after I removed the license entries and created the license link in the meta-st-stm32mp-addons/conf/eula directory (this is the only way I can make it work). I added back the lines you've mentioned and now it looks like this:
# We have a conf and classes directory, add to BBPATH
BBPATH .= ":${LAYERDIR}"
# We have recipes-* directories, add to BBFILES
BBFILES += "${LAYERDIR}/recipes-*/*/*.bb \
${LAYERDIR}/recipes-*/*/*.bbappend"
BBFILE_COLLECTIONS += "meta-mylayer"
BBFILE_PATTERN_meta-mylayer = "^${LAYERDIR}/"
BBFILE_PRIORITY_meta-mylayer = "7"
EULA_FILE_ST_stm32mpmylayer = "${LAYERDIR}/conf/eula/${MACHINE}"
EULA_FILE_ST_MD5SUM_stm32mpmylayer = "8b505090fb679839cefbcc784afe8ce9"
#Inform bitbake for adding another location to search for licenses
LICENSE_PATH += "${LAYERDIR}/files/licenses"
# Set a variable to get the STM32MP MX BSP location
STM32MP_MYLAYER_BASE = "${LAYERDIR}"
# This should only be incremented on significant changes that may
# cause compatibility issues with other layers
LAYERVERSION_meta-mylayer = "1"
LAYERSERIES_COMPAT_meta-mylayer = "thud"
LAYERDEPENDS_meta-mylayer = "stm-st-stm32mp-mx"
my machine conf has also the line:
MACHINEOVERRIDES .= ":stm32mpmylayer"
However I still have the same error and bitbake looks for the license file in the meta-st/meta-st-stm32mp-addons/conf/eula/ directory. Are there some requirements regarding the layer and the machine names (for example the *-layer suffix in the layer name)? My layer is called meta-mylayer and is located in the meta-st directory.
Krzysztof
2019-12-04 4:39 AM
Hi @Community member
To match with this layer.conf EULA link has to be done inside your own layer.
As per describe in section 2.3 of the wiki https://wiki.st.com/stm32mpu/wiki/How_to_compile_the_device_tree_with_the_Distribution_Package#Associate_EULA_with_the_new_demo_machine
First copy /conf/eula from Adds-on to your layer and then do the link
Olivier
2019-12-04 4:47 AM
That's right - I have already copied the eula directory to my own layer and created a link there, but bitbake still checks for it in the meta-st-stm32mp-addons layer. The only way I can get rid of this error is to create the link with my machine name in the meta-st-stm32mp-addons.
Krzysztof
2019-12-04 5:25 AM
Can you please share result of :
bitbake -e | grep ^EULA_FILE_ST
and
bitbake-layers show-layers
Thanks
Olivier