cancel
Showing results for 
Search instead for 
Did you mean: 

Android support

Hello,

Could you explain the reason why Android is not supported on the STM32MP157C-DK2?

I can't find any instructions how to install an Android image on the target? The following example references the coprocessor example for A7 and M4 cores, but misses how this is done:-

https://wiki.st.com/stm32mpu/wiki/STM32MP1_Developer_Package_for_Android

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Olivier GALLIEN
ST Employee

Hi @moredatalesscenter​ 

Android does not fit to DK2 because there is not enough DDR ( 1GB required) .

Guideline to install Android on target is there :

https://wiki.st.com/stm32mpu/wiki/How_to_populate_boards_for_Android

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Ah. The board features suggest it's 4 Gbit DDR3L, 16 bits.

Indeed ..which mean 512MBytes. ;)

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Can packages be selectively removed to create a barebones distribution that will fit into 0.5GB?

Nicolas L
ST Employee

Android from AOSP can work with 512MBytes but with an impact on the overall performance (swap has a huge impact).

It's then required to limit the memory usage to the maximum:

1- limit the display resolution on the device

2- limit the number of packages started (remove all unnecessary packages which can means patching the system server to avoid starting them (ex: Telecom))

3- applications (packages) including the Launcher shall be developed considering memory usage (no animation, simple layouts (ex: use ConstrainLayout), avoid too much activity swap...)

At the end, it depends on the kind of device targeted (ex: wear device with small screen can work easily with 512MBytes DDR)