2021-09-18 2:46 AM
I'm build an image for Azure IOT on STM32MP157C-DK2, following this tutorial: https://wiki.st.com/stm32mpu/wiki/How_to_integrate_Azure_IoT_Edge_on_OpenSTLinux
but I have follow error:
| error: attributes are not yet allowed on `if` expressions
| --> /usr/src/debug/iotedge-daemon/1.1.6-r0/iotedge-1.1.6/vendor/sysinfo/src/utils.rs:27:5
| |
| 27 | #[allow(clippy::identity_conversion)]
| | ^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^
|
| error: aborting due to previous error
|
| error: could not compile `sysinfo`.
There is a possible solution?
Looking a similar issues, it seem a problem of version of Rust: https://github.com/Frederick888/git-credential-keepassxc/issues/12
There is a way to udate the Rust version used for build?
2021-09-19 11:18 AM
Hello,
have you installed all the dependencies needed for the Distribution package building?
Br,
2021-09-19 1:05 PM
Yes, I did. once I make follow command:
DISTRO=openstlinux-weston MACHINE=stm32mp1 source layers/meta-st/scripts/envsetup.sh
it asked me all dependencies. I installed them and after when I re launch the command, it say was all ok and I started the build.
Can I ask witch versions of repository of those layers are tested in the tutorial?
PC $>git clone -b dunfell https://github.com/Azure/meta-iotedge.git
PC $>git clone git://github.com/meta-rust/meta-rust.git
PC $>git clone -b dunfell git://git.yoctoproject.org/meta-virtualization
I noticed that the are some update in repository meta-iotedge.git in date after the last update of article.
2021-09-19 11:31 PM
Hello @EBelt.1
to build Rust packages, I am using this repository:
https://github.com/rust-embedded/meta-rust-bin
It may help you. This layer supports Rust 1.54 and it is easy to upgrade to 1.55 (use the script build-new-version.sh).
Best regards,
--JM
2021-09-20 12:35 AM
Thank you for your support. Just to understand (I'm pretty new to this builds), you say to replace those steps:
git clone git://github.com/meta-rust/meta-rust.git
bitbake-layers add-layer [your STM32MP1 Distribution path]/meta-rust/
with:
git clone https://github.com/rust-embedded/meta-rust-bin
bitbake-layers add-layer [your STM32MP1 Distribution path]/meta-rust-bin/
About that, I looking that has a specific branch for dunfell, instead meta-rust-bin has only for dizzy and zeus. What branch should I use? The master branch?
2021-09-20 12:56 AM
@EBelt.1
Yes, you can use the master branch. The compatibility layer as defined in conf/layer.conf includes dunfell.
Best regards,
--JM
2021-09-20 9:41 AM
I tried to use meta-rust-bin, but the layer iot edge looks to depend on meta-rust:
ERROR: Layer 'meta-iotedge' depends on layer 'rust-layer', but this layer is not enabled in your configuration
2021-09-20 11:21 PM
Hello @EBelt.1
ok, I was not aware of this dependency. Too bad, the meta-rust-bin layer is quite quick ;)
To come back to your initial question, you can update the Rust compiler version by setting the variable RUST_VERSION = "1.55.0" (or other values) in your local.conf file.
About the versions used in the tutorial:
meta-iotedge : branch dunfell : commit 6840cf2afb51b4f2c535a05d5635736652f664f7
meta-virtualization : branch dunfell : commit 502b81ae3ae11bf4d889b7eff6239fb9e6c55994
meta-rust : branch master : commit e4d25b98083bcecb94df6ee189a165d63ede7f3d
The tutorial has been validated against the delivery ecosystem release v3.0.0 so be sure to used it.
Best regards,
--JM
2021-09-22 3:48 PM
Thank you for the suggestion! I added RUST_VERSION = "1.55.0" to local.conf and aligned layers as suggested, but I had an error on building virtualitation (a repo was not found), but moving virtualitation to lastest everything work fine.
So, my final set was:
meta-iotedge : branch dunfell : commit 6840cf2afb51b4f2c535a05d5635736652f664f7
meta-rust : branch master : commit e4d25b98083bcecb94df6ee189a165d63ede7f3d
meta-virtualization : branch dunfell : latest commit
RUST_VERSION = "1.55.0" in local.conf
and I successfully build the image and connected to IOTedge.
I noticed that the version of Iotedge is 1.1, that has know issues. Is it possible to update to version 1.2 of iotedge?
2021-09-22 10:54 PM
Hello @EBelt.1
I am happy you successfully built your image! That's a good point!
About your last question to migrate from 1.1 to 1.2 for the layer iotedge, I don't know. I think you should make an attempt on your side and select this version in your cloned repository and re-do the build.
Best regards,
--JM