cancel
Showing results for 
Search instead for 
Did you mean: 

Compiling azure sphere os for the stm32mp157D-DK1.

RLati.1
Associate

Good day,

Has anyone been able to compile Azure Sphere OS for the STM32MP157D-DK1.

I have the yocto environment configured, and I am able to build a vanilla embedded Linux image, but when I add the azure bblayers to the build. the build fails.

I also tried building the OS with the provided build-os.sh script, it built successfully but I was not able to get the dev board to boot.

Kind regards,

Rayaan

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Olivier GALLIEN
ST Employee

Hi @RLati.1​ ,

Could you elaborate further what you want to do ?

Could you point the azure bblayers you mention ?

Do you want to run Azure Sphere A7 side or M4 side ?

I can't get access to your link. Please attach it to your next comment.

Thanks,

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.