2025-03-25 3:44 AM
Hi,
I'm trying to run the whole ST-Linux-stuff on one core only to have the other one available for a time-consuming application. However, it seems the kernel-parameter isolcpus is not used, dmesg gives an output
[ 0.000000] Kernel command line: root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw earlycon console=ttySTM0,115200 isolcpus=0
[ 0.000000] Unknown kernel command line parameters "isolcpus=0", will be passed to user space.
[ 2.309368] isolcpus=0
The message is correct, also with this parameter set, the processes are spread over all cores.
What could be the problem here?
Thanks!
Solved! Go to Solution.
2025-03-28 2:11 AM
Hello @HMüll.4 ,
I find it strange that you have this warning on your second line. I have it too using the same command line parameter as you have. However, using 1 as parameter, the warning is not here anymore and it seems to have the expected result.
Can you please make a try with isolcpus=1 instead of 0 ?
Kind regards,
Erwan.
2025-03-28 2:11 AM
Hello @HMüll.4 ,
I find it strange that you have this warning on your second line. I have it too using the same command line parameter as you have. However, using 1 as parameter, the warning is not here anymore and it seems to have the expected result.
Can you please make a try with isolcpus=1 instead of 0 ?
Kind regards,
Erwan.