2022-06-22 7:45 AM
Hello,
When I plugged the IMX477 on a USB port and I have the following msg:
[ 7307.355686] usb 2-1.3: new high-speed USB device number 5 using ehci-platform
[ 7307.519593] uvcvideo: Found UVC 1.00 device Arducam IMX477 HQ Camera (0c45:636d)
[ 7307.534627] input: Arducam IMX477 HQ Camera: Arduc as /devices/platform/soc/5800d000.usbh-ehci/usb2/2-1/2-1.3/2-1.5
[ 7307.550269] usb 2-1.3: 3:1: cannot get freq at ep 0x84
[ 7308.295030] usb 2-1.3: 3:1: cannot get freq at ep 0x84
[ 7308.349280] usb 2-1.3: 3:1: cannot get freq at ep 0x84
2022-07-10 10:42 PM
Hi @JACQUES Jérôme ,
I'm not expert but I understand that such device may require some specific driver/support which does not looks to be by default in OpenSTLinux.
Which version of ecosystem are you using ?
Olivier
2022-07-11 12:40 AM
Hi Olivier,
Thanks for you interest !
I'm using the 2.1. I see there is the 4.0 version maybe ....
A question Olivier, do you work in Sophia Antipolis ?
If yes, is it possible to have a meeting ?
Best regards,
Jérôme
2022-07-11 1:06 AM