2025-03-18 8:00 AM - edited 2025-03-18 8:01 AM
Hi everyone,
We have developed a custom board based on stm32mp157 mpu. We have used openstlinux distribution and the branch is "kirkstone". We have interfaced edt_ft5x06 display. Display is working perfectly fine but problem arises when we try to interact with the touch. It is completely unresponsive. With "evtest" in Linux kernel I do not see any touch event. Devicetree entry for my touch-screen is following:
touchscreen@38 {
compatible ="edt,edt-ft5406";
reg = <0x38>;
interrupts = <2 2>;
interrupt-parent = <&gpiof>;
interrupt-controller;
touchscreen-size-x = <480>;
touchscreen-size-y = <800>;
vcc-supply = <&v3v3>;
iovcc-supply = <&v3v3>;
status = "okay";
};
If I look thorough the dmesg, then I get following entry:
[ 2.081938] input: EP0700M12 as /devices/platform/soc/40012000.i2c/i2c-0/0-0038/input/input0
Also I have following entry for the interrupt:
cat /proc/interrupts
CPU0 CPU1
26: 22514 70457 GIC-0 27 Level arch_timer
30: 0 0 GIC-0 67 Level 44004000.spi
31: 0 0 GIC-0 43 Level dma1chan0
32: 0 0 GIC-0 44 Level dma1chan1
33: 0 0 GIC-0 45 Level dma1chan2
34: 382 0 GIC-0 46 Level dma1chan3
35: 0 0 GIC-0 47 Level dma1chan4
36: 0 0 GIC-0 48 Level dma1chan5
37: 0 0 GIC-0 49 Level dma1chan6
38: 0 0 GIC-0 79 Level dma1chan7
41: 2 0 GIC-0 154 Level 58000000.dma-controller
42: 0 0 GIC-0 124 Level 58003000.spi
43: 68928 0 GIC-0 81 Level mmci-pl18x (cmd)
44: 1181 0 GIC-0 156 Level mmci-pl18x (cmd)
45: 11211 0 GIC-0 93 Level eth0
46: 1 0 GIC-0 106 Level ohci_hcd:usb2
47: 455 0 GIC-0 120 Level 5a001000.display-controller
48: 0 0 GIC-0 121 Level 5a001000.display-controller
53: 37 0 stm32-exti-h-direct 32 Level 40018000.serial
54: 0 0 stm32-exti-h-direct 70 Level eth0
55: 26 0 stm32-exti-h-direct 43 Level ehci_hcd:usb1
56: 0 0 stm32-exti-h-direct 19 Level 5c004000.rtc
57: 58 0 stm32-exti-h-direct 21 Level 40012000.i2c
58: 0 0 GIC-0 64 Level 40012000.i2c
59: 0 0 stm32gpio 2 Edge edt-ft5406
60: 0 0 stm32-exti-h-direct 25 Level 40015000.i2c
61: 0 0 GIC-0 140 Level 40015000.i2c
IPI0: 0 0 CPU wakeup interrupts
IPI1: 0 0 Timer broadcast interrupts
IPI2: 36 72 Rescheduling interrupts
IPI3: 4883 77663 Function call interrupts
IPI4: 0 0 CPU stop interrupts
IPI5: 0 0 IRQ work interrupts
IPI6: 0 0 completion interrupts
Err: 0
I tried possible solutions, but could not get it to work. Can anyone tell me what is the reason for this behavior? Thanks a lot.