2019-07-30 8:30 AM
Hi,
I am using the STM32MP157C-DK2 and so far i manged to make FREERTOS work flawlessly with OpenAMP and the tracing printf functions. I can insert breakpoint at any point without a problem. However, i start having issues when i declare a semaphore or a mutex in the function MX_FREERTOS_Init().
Here is my main.c file:
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
*/
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "cmsis_os.h"
#include "ipcc.h"
#include "openamp.h"
#include "gpio.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "stm32mp15xx_disco.h"
#include "log.h"
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
void MX_FREERTOS_Init(void);
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
if(IS_ENGINEERING_BOOT_MODE())
{
SystemClock_Config();
}
/* IPCC initialisation */
MX_IPCC_Init();
/* OpenAmp initialisation ---------------------------------*/
MX_OPENAMP_Init(RPMSG_REMOTE, NULL);
/* Initialize all configured peripherals */
MX_GPIO_Init();
__HAL_RCC_HSEM_CLK_ENABLE();
BSP_LED_Init(LED7);
BSP_LED_Init(LED5);
/* Call init function for freertos objects (in freertos.c) */
MX_FREERTOS_Init();
/* Start scheduler */
osKernelStart();
/* We should never get here as control is now taken by the scheduler */
/* Infinite loop */
while (1)
{
}
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
/** Configure LSE Drive Capability
*/
HAL_PWR_EnableBkUpAccess();
__HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_MEDIUMHIGH);
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_LSI
|RCC_OSCILLATORTYPE_HSE|RCC_OSCILLATORTYPE_LSE;
RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS_DIG;
RCC_OscInitStruct.LSEState = RCC_LSE_ON;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = 16;
RCC_OscInitStruct.HSIDivValue = RCC_HSI_DIV1;
RCC_OscInitStruct.LSIState = RCC_LSI_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLL12SOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 3;
RCC_OscInitStruct.PLL.PLLN = 81;
RCC_OscInitStruct.PLL.PLLP = 1;
RCC_OscInitStruct.PLL.PLLQ = 2;
RCC_OscInitStruct.PLL.PLLR = 2;
RCC_OscInitStruct.PLL.PLLFRACV = 0x800;
RCC_OscInitStruct.PLL.PLLMODE = RCC_PLL_FRACTIONAL;
RCC_OscInitStruct.PLL.RPDFN_DIS = RCC_RPDFN_DIS_DISABLED;
RCC_OscInitStruct.PLL.TPDFN_DIS = RCC_TPDFN_DIS_DISABLED;
RCC_OscInitStruct.PLL2.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL2.PLLSource = RCC_PLL12SOURCE_HSE;
RCC_OscInitStruct.PLL2.PLLM = 3;
RCC_OscInitStruct.PLL2.PLLN = 66;
RCC_OscInitStruct.PLL2.PLLP = 2;
RCC_OscInitStruct.PLL2.PLLQ = 1;
RCC_OscInitStruct.PLL2.PLLR = 1;
RCC_OscInitStruct.PLL2.PLLFRACV = 0x1400;
RCC_OscInitStruct.PLL2.PLLMODE = RCC_PLL_FRACTIONAL;
RCC_OscInitStruct.PLL2.RPDFN_DIS = RCC_RPDFN_DIS_DISABLED;
RCC_OscInitStruct.PLL2.TPDFN_DIS = RCC_TPDFN_DIS_DISABLED;
RCC_OscInitStruct.PLL3.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL3.PLLSource = RCC_PLL3SOURCE_HSE;
RCC_OscInitStruct.PLL3.PLLM = 2;
RCC_OscInitStruct.PLL3.PLLN = 34;
RCC_OscInitStruct.PLL3.PLLP = 2;
RCC_OscInitStruct.PLL3.PLLQ = 17;
RCC_OscInitStruct.PLL3.PLLR = 37;
RCC_OscInitStruct.PLL3.PLLRGE = RCC_PLL3IFRANGE_1;
RCC_OscInitStruct.PLL3.PLLFRACV = 6660;
RCC_OscInitStruct.PLL3.PLLMODE = RCC_PLL_FRACTIONAL;
RCC_OscInitStruct.PLL3.RPDFN_DIS = RCC_RPDFN_DIS_DISABLED;
RCC_OscInitStruct.PLL3.TPDFN_DIS = RCC_TPDFN_DIS_DISABLED;
RCC_OscInitStruct.PLL4.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL4.PLLSource = RCC_PLL4SOURCE_HSE;
RCC_OscInitStruct.PLL4.PLLM = 4;
RCC_OscInitStruct.PLL4.PLLN = 99;
RCC_OscInitStruct.PLL4.PLLP = 6;
RCC_OscInitStruct.PLL4.PLLQ = 8;
RCC_OscInitStruct.PLL4.PLLR = 8;
RCC_OscInitStruct.PLL4.PLLRGE = RCC_PLL4IFRANGE_0;
RCC_OscInitStruct.PLL4.PLLFRACV = 0;
RCC_OscInitStruct.PLL4.PLLMODE = RCC_PLL_INTEGER;
RCC_OscInitStruct.PLL4.RPDFN_DIS = RCC_RPDFN_DIS_DISABLED;
RCC_OscInitStruct.PLL4.TPDFN_DIS = RCC_TPDFN_DIS_DISABLED;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** RCC Clock Config
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_ACLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_PCLK3|RCC_CLOCKTYPE_PCLK4
|RCC_CLOCKTYPE_PCLK5|RCC_CLOCKTYPE_MPU;
RCC_ClkInitStruct.MPUInit.MPU_Clock = RCC_MPUSOURCE_PLL1;
RCC_ClkInitStruct.MPUInit.MPU_Div = RCC_MPU_DIV2;
RCC_ClkInitStruct.AXISSInit.AXI_Clock = RCC_AXISSOURCE_PLL2;
RCC_ClkInitStruct.AXISSInit.AXI_Div = RCC_AXI_DIV1;
RCC_ClkInitStruct.MCUInit.MCU_Clock = RCC_MCUSSOURCE_PLL3;
RCC_ClkInitStruct.MCUInit.MCU_Div = RCC_MCU_DIV1;
RCC_ClkInitStruct.APB4_Div = RCC_APB4_DIV2;
RCC_ClkInitStruct.APB5_Div = RCC_APB5_DIV4;
RCC_ClkInitStruct.APB1_Div = RCC_APB1_DIV2;
RCC_ClkInitStruct.APB2_Div = RCC_APB2_DIV2;
RCC_ClkInitStruct.APB3_Div = RCC_APB3_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct) != HAL_OK)
{
Error_Handler();
}
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USBO|RCC_PERIPHCLK_DDRPHYC
|RCC_PERIPHCLK_SAI2|RCC_PERIPHCLK_RTC
|RCC_PERIPHCLK_LTDC|RCC_PERIPHCLK_UART24
|RCC_PERIPHCLK_SPI23|RCC_PERIPHCLK_SDMMC12
|RCC_PERIPHCLK_I2C12|RCC_PERIPHCLK_ADC
|RCC_PERIPHCLK_I2C46|RCC_PERIPHCLK_CEC
|RCC_PERIPHCLK_RNG1|RCC_PERIPHCLK_CKPER;
PeriphClkInit.I2c12ClockSelection = RCC_I2C12CLKSOURCE_HSI;
PeriphClkInit.I2c46ClockSelection = RCC_I2C46CLKSOURCE_HSI;
PeriphClkInit.Sai2ClockSelection = RCC_SAI2CLKSOURCE_PLL3_Q;
PeriphClkInit.Spi23ClockSelection = RCC_SPI23CLKSOURCE_PLL3_Q;
PeriphClkInit.Uart24ClockSelection = RCC_UART24CLKSOURCE_HSI;
PeriphClkInit.EthClockSelection = RCC_ETHCLKSOURCE_PLL4;
PeriphClkInit.DsiClockSelection = RCC_DSICLKSOURCE_PHY;
PeriphClkInit.CkperClockSelection = RCC_CKPERCLKSOURCE_HSE;
PeriphClkInit.Rng1ClockSelection = RCC_RNG1CLKSOURCE_LSI;
PeriphClkInit.UsbphyClockSelection = RCC_USBPHYCLKSOURCE_HSE;
PeriphClkInit.UsboClockSelection = RCC_USBOCLKSOURCE_PHY;
PeriphClkInit.CecClockSelection = RCC_CECCLKSOURCE_LSE;
PeriphClkInit.Lptim1ClockSelection = RCC_LPTIM1CLKSOURCE_OFF;
PeriphClkInit.Lptim23ClockSelection = RCC_LPTIM23CLKSOURCE_OFF;
PeriphClkInit.Lptim45ClockSelection = RCC_LPTIM45CLKSOURCE_OFF;
PeriphClkInit.AdcClockSelection = RCC_ADCCLKSOURCE_PER;
PeriphClkInit.RTCClockSelection = RCC_RTCCLKSOURCE_LSE;
PeriphClkInit.TIMG1PresSelection = RCC_TIMG1PRES_DEACTIVATED;
PeriphClkInit.TIMG2PresSelection = RCC_TIMG2PRES_DEACTIVATED;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
Error_Handler();
}
/** Set the HSE division factor for RTC clock
*/
__HAL_RCC_RTC_HSEDIV(24);
}
And here is my app_freertos.c
Solved! Go to Solution.
2019-07-30 8:52 AM
Hello,
could you please precise if you are using SW4STM32 (i.e. GDB/OpenOCD debug) or another debugger ?
There is a separate thread which sound similar : https://community.st.com/s/question/0D50X0000B422in/stm32mp1-freertos-debug-issue
Is reducing the optimization level solve your issue ?
Seems linked to the way GDB manage the debug and the way FreeRTOS manage the stack pointers.
2019-07-30 8:31 AM
And here is my app_freertos.c:
/**
******************************************************************************
* File Name : app_freertos.c
* Description : Code for freertos applications
******************************************************************************
*/
/* Includes ------------------------------------------------------------------*/
#include "FreeRTOS.h"
#include "task.h"
#include "main.h"
#include "cmsis_os.h"
/* Private includes ----------------------------------------------------------*/
#include "stm32mp15xx_disco.h"
#include "log.h"
#include "openamp.h"
#include <stdio.h>
/* Private define ------------------------------------------------------------*/
#define MAX_BUFFER_SIZE RPMSG_BUFFER_SIZE
/* Private variables ---------------------------------------------------------*/
VIRT_UART_HandleTypeDef hvuart0;
__IO FlagStatus VirtUart0RxMsg = RESET;
uint8_t VirtUart0ChannelBuffRx[MAX_BUFFER_SIZE];
uint16_t VirtUart0ChannelRxSize = 0;
osThreadId TaskIdleHandle;
osThreadId TaskLedBlinkHandle;
osThreadId TaskVUART0Handle;
osMessageQId QueueTxMP1Handle;
osMessageQId QueueRxMP1Handle;
osMutexId myMutex01Handle;
osSemaphoreId myBinarySem01Handle;
/* Private function prototypes -----------------------------------------------*/
void VIRT_UART0_RxCpltCallback(VIRT_UART_HandleTypeDef *huart);
void StartTaskIdle(void const * argument);
void StartTaskLedBlink(void const * argument);
void StartTaskVUART0(void const * argument);
void MX_FREERTOS_Init(void); /* (MISRA C 2004 rule 8.1) */
/* GetIdleTaskMemory prototype (linked to static allocation support) */
void vApplicationGetIdleTaskMemory( StaticTask_t **ppxIdleTaskTCBBuffer, StackType_t **ppxIdleTaskStackBuffer, uint32_t *pulIdleTaskStackSize );
static StaticTask_t xIdleTaskTCBBuffer;
static StackType_t xIdleStack[configMINIMAL_STACK_SIZE];
void vApplicationGetIdleTaskMemory( StaticTask_t **ppxIdleTaskTCBBuffer, StackType_t **ppxIdleTaskStackBuffer, uint32_t *pulIdleTaskStackSize )
{
*ppxIdleTaskTCBBuffer = &xIdleTaskTCBBuffer;
*ppxIdleTaskStackBuffer = &xIdleStack[0];
*pulIdleTaskStackSize = configMINIMAL_STACK_SIZE;
/* place for user code */
}
/**
* @brief FreeRTOS initialization
* @param None
* @retval None
*/
void MX_FREERTOS_Init(void) {
osStatus status;
/* Create the mutex(es) */
/* definition and creation of myMutex01 */
osMutexDef(myMutex01);
myMutex01Handle = osMutexCreate(osMutex(myMutex01));
//status = osMutexDelete (myMutex01Handle);
//if(status != osOK)
//{
// log_err("Mutex delete failed");
//}
/* Create the semaphores(s) */
/* definition and creation of myBinarySem01 */
osSemaphoreDef(myBinarySem01);
myBinarySem01Handle = osSemaphoreCreate(osSemaphore(myBinarySem01), 1);
//status = osSemaphoreDelete (myBinarySem01Handle);
//if(status != osOK)
//{
// log_err("Semaphore delete failed");
//}
/* Create the queue(s) */
/* definition and creation of QueueTxMP1 */
osMessageQDef(QueueTxMP1, 128, uint8_t);
QueueTxMP1Handle = osMessageCreate(osMessageQ(QueueTxMP1), NULL);
/* definition and creation of QueueRxMP1 */
osMessageQDef(QueueRxMP1, 128, uint8_t);
QueueRxMP1Handle = osMessageCreate(osMessageQ(QueueRxMP1), NULL);
/* Create the thread(s) */
/* definition and creation of TaskIdle */
osThreadDef(TaskIdle, StartTaskIdle, osPriorityIdle, 0, 128);
TaskIdleHandle = osThreadCreate(osThread(TaskIdle), NULL);
/* definition and creation of TaskLedBlink */
osThreadDef(TaskLedBlink, StartTaskLedBlink, osPriorityNormal, 0, 128);
TaskLedBlinkHandle = osThreadCreate(osThread(TaskLedBlink), NULL);
/* definition and creation of TaskVUART0 */
osThreadDef(TaskVUART0, StartTaskVUART0, osPriorityNormal, 0, 128);
TaskVUART0Handle = osThreadCreate(osThread(TaskVUART0), NULL);
}
/**
* @brief Function implementing the TaskIdle thread.
* @param argument: Not used
* @retval None
*/
void StartTaskIdle(void const * argument)
{
/* Infinite loop */
for(;;)
{
osDelay(1);
}
}
/**
* @brief Function implementing the TaskLedBlink thread.
* @param argument: Not used
* @retval None
*/
void StartTaskLedBlink(void const * argument)
{
log_info("TaskLedBlink Started");
log_info("TaskLedBlink Initialization Complete");
/* Infinite loop */
for(;;)
{
BSP_LED_Toggle(LED7);
osDelay(100);
}
}
/**
* @brief Function implementing the TaskVUART0 thread.
* @param argument: Not used
* @retval None
*/
void StartTaskVUART0(void const * argument)
{
log_info("TaskVUART0 Started");
if (VIRT_UART_Init(&hvuart0) != VIRT_UART_OK) {
log_err("VIRT_UART_Init UART0 failed");
Error_Handler();
}
/*Need to register callback for message reception by channels*/
if (VIRT_UART_RegisterCallback(&hvuart0, VIRT_UART_RXCPLT_CB_ID,
VIRT_UART0_RxCpltCallback) != VIRT_UART_OK) {
log_err("VIRT_UART_RegisterCallback UART0 failed");
Error_Handler();
}
log_info("TaskVUART0 Initialization Complete");
/* Infinite loop */
for(;;)
{
OPENAMP_check_for_message();
if (VirtUart0RxMsg) {
VirtUart0RxMsg = RESET;
VIRT_UART_Transmit(&hvuart0, VirtUart0ChannelBuffRx, VirtUart0ChannelRxSize);
}
osDelay(1);
}
}
/* Private application code --------------------------------------------------*/
void VIRT_UART0_RxCpltCallback(VIRT_UART_HandleTypeDef *huart)
{
log_info("Msg received on VIRTUAL UART0 channel: %s", (char *) huart->pRxBuffPtr);
/* copy received msg in a variable to sent it back to master processor in main infinite loop*/
VirtUart0ChannelRxSize = huart->RxXferSize < MAX_BUFFER_SIZE? huart->RxXferSize : MAX_BUFFER_SIZE-1;
memcpy(VirtUart0ChannelBuffRx, huart->pRxBuffPtr, VirtUart0ChannelRxSize);
VirtUart0RxMsg = SET;
}
2019-07-30 8:50 AM
Here is some images showing what i am experiencing:
This image shows what i see when I initialize the mutex (but do not use it, as seen in the app_freertos.c file in the previous post) and i am stepping inside the function MX_FREERTOS_Init before the scheduler is called. We can see that i placed a break point inside the Led blink task and that the dissasembly seems ok for that part of the code:
Then, when i hit the "resume", it hits the breakpoint and the disassembly seems ok. But when i press resume again, it should hit back the same break point 100ms later...but it hangs there and its over.
The board is now bricked and has to be reset before i can launch a new debug session. Here in this last image, i launch the debug session with no breakpoint. The code is running fine (the led is blinking), but when i place a breakpoint at the same place, i get a weird disassembly. Also i cannot "resume" because it hangs there.
I tried declaring the mutex/semaphone, and delete them immediately after, and it does the same thing. The only wait to be able to debug with break points is to not initialize any semaphone or mutex.
I cannot continue my projet without mutex or semaphore...as i need task synchronisation.
Also i observed the same problem when using Queues. There are using semaphore under the hood and when ever i insert a breakpoint, it hangs.
2019-07-30 8:52 AM
Hello,
could you please precise if you are using SW4STM32 (i.e. GDB/OpenOCD debug) or another debugger ?
There is a separate thread which sound similar : https://community.st.com/s/question/0D50X0000B422in/stm32mp1-freertos-debug-issue
Is reducing the optimization level solve your issue ?
Seems linked to the way GDB manage the debug and the way FreeRTOS manage the stack pointers.
2019-07-30 10:26 AM
Hi Patrick,
I am using SW4STM32 and it looks like it works when i remove the option "optimize for debugging" and set it to "None":
I will move foward and see if it still works when i start using the declared mutex and semaphore.
Thanks!
2019-07-30 2:13 PM
Ok so here is the sad part:
When i use "None" in Optimization level, OpenAMP works erratically and end up crashing!
But when i use "Optimize for Debug", everything works (OpenAmp, semaphores, mutexes, queues, etc.) but i cannot insert a breakpoint!
This is a major issue for debugging!