cancel
Showing results for 
Search instead for 
Did you mean: 

In the STM32MP157C to go to the DFU mode is it necessary that the Vbus pine is connected or can it be done via the firmware??

KS.2
Associate III
 
1 REPLY 1
PatrickF
ST Employee

Hi,

I confirm BootROM does not need neither VBUS nor ID pins to work in DFU mode.

For uBoot and Kernel, please see DT settings in https://wiki.st.com/stm32mpu/wiki/How_to_configure_U-Boot_for_your_board#USB_OTG_node

Regards.

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.