2020-12-02 07:27 AM
I have the latest version of ST-Link Utility (ver. 4.6.0) on Windows 10 and the latest firmware (V2.J37.S7), both of which I downloaded yesterday. My co-worker has ST-Link Utility ver. 3.7.0 on Windows 7 and firmware V2.J24.S7 and he has no trouble writing to the device.
I'm having several other errors:
Blank check almost always fails. When I check the memory location where Blank Check fails, it looks right.
Sometimes (maybe 1 in 6 tries) the first file I try to load does load. But the second file NEVER loads. I get this error: Programming error @ 0x0800344C! (the memory address is always different.)
Read Out Protection is Disabled and no Flash sectors are protected.
I am using Program and Verify with Verify while programming selected.
Can you provide any assistance in programming this device? Is it possible to get the older version of ST-Link Utility and the older firmware?
2020-12-02 08:16 AM
Determined that the issues were caused by a bad cable.