2023-06-01 11:28 AM
The STM32MP1 example code on github targets the STM32MP157C on the STM32MP157C-DK2 and STM32MP157C-EV1 eval boards, however both of those boards are obsolete. I am using the STM23MP157D-DK1 eval board.
How do I port the example code so that it targets the correct chip and eval board?
Specifically, I am trying looking at the OpenAMP example code:
https://github.com/STMicroelectronics/STM32CubeMP1/
Thank you,
Owen
2023-06-02 1:18 AM
Hello @OMurp.1 ,
Basically, it should not be very different. Platforms are really closed to each other, you just do not have native display on DK1 if I remember well, and maybe some minor functionalities also.
If you already have a BSP ready, and a CubeFW package in phase with the kernel that runs on your A7 cortex, I do not see blocker for you to setup your example.
Did you face some trouble with it ?
Kind regards,
Erwan.
2023-06-02 6:22 AM
Hi Erwan,
I ended up making a new project targeting the DK1 setup, using CubeMX with OpenAMP enabled. I was able to copy all the relevant code over to my new project, and it seems to work just fine. Thanks for the response.
-Owen