2021-01-11 5:32 AM
Good morning,
I'm working on a C++ project to collect data from a peripheral sensor using the STM32MP157C-DK2.
The estimated amount of data is at least 100 MB, so I have to use the DDR3 to store these data and then trasmit them over Ethernet using at the moment ONLY Cortex-A7 (no M4).
The project is write in C++ language and NOT using CubeMX, so I'm asking how can I activate and use the DDR3.
I've read some tutorials/documents from various sources:
# https://www.st.com/en/microcontrollers-microprocessors/stm32mp157.html#documentation
# https://wiki.st.com/stm32mpu/wiki/How_to_exchange_large_data_buffers_with_the_coprocessor_-_example
and consequently I wrote the code (you will find it here attached with the dts in the card partition called "bootfs"), but I always receive the cout message "Mapping param failed.".
What I've to modify in the main code and, eventually, how/where can I add/modify the missing dts data to the MP1?
2021-01-19 6:29 AM
Hi @FrancoB ,
Sorry, I'm a bit puzzled with description of your problem.
I understand you would like to achieve Ethernet transfer of data from a peripheral sensor on A7 Linux side right ?
M4 and A7 to M4 communication not involved right ?
But you refer to
# https://wiki.st.com/stm32mpu/wiki/How_to_exchange_large_data_buffers_with_the_coprocessor_-_example
Which demonstrate only buffer exchange between A7 and M4 ...
Can you please clarify ?
Thx
Olivier
2021-01-19 7:43 AM
2021-01-22 1:21 AM
Your description is right, Oliver. The reason I've shared those links is because those are the principal tutorial references I've get to better understand how to send the data from a device to another (in this case M4 <-> A7).