2022-11-22 11:02 PM
Hello,
I wants to bitbake ot-br-posix with OT_THREAD_VERSION=1.1, Modified the ot-br-posix_git.bb file, add -DOT_THREAD_VERSION=1.1 in this file. But result is ot-br-posix using Thread Version 1.2
Does somebody know how to solve this issue
Many thanks.
B.R
Frank
2022-11-28 9:28 PM
Hi JM,
I missed something when issue ./script/bootstrap
WEB_GUI=1 NFRA_IF_NAME=wlan0 ./script/bootstrap
Should add NFRA_IF_NAME=***
Sorry,
Best Regards
Frank
2022-12-02 7:22 AM
Hi @Community member
I made some significant progress as I can see these outputs in my /var/log/messages:
Dec 2 16:09:41 stm32mp1 user.info otbr-agent[1032]: [INFO]-UTILS---: Running 0.3.0-ad6822257f-dirty
Dec 2 16:09:41 stm32mp1 user.info otbr-agent[1032]: [INFO]-UTILS---: Thread version: 1.1.1
Dec 2 16:09:41 stm32mp1 user.info otbr-agent[1032]: [INFO]-UTILS---: Thread interface: wpan0
Dec 2 16:09:41 stm32mp1 user.info otbr-agent[1032]: [INFO]-UTILS---: Backbone interface: wlan0
Dec 2 16:09:41 stm32mp1 user.info otbr-agent[1032]: [INFO]-UTILS---: Radio URL: spinel+hdlc+uart:///dev/ttyUSB0
Dec 2 16:09:41 stm32mp1 user.info otbr-agent[1032]: [INFO]-UTILS---: Radio URL: trel://eth0
Dec 2 16:09:43 stm32mp1 user.crit otbr-agent[1032]: 49d.17:07:12.290 [C] Platform------: BSD TCP function() at radio_spinel_impl.hpp:2236: RadioSpinelNoResponse
To achieve this result, I introduced a bbappend recipe:
FILESEXTRAPATHS:prepend := "${THISDIR}/ot-br-posix:"
SRC_URI += "\
file://manage-ot-thread-version-1.1.patch \
"
# openthread/repo/src/cli/cli.cpp:1786:18: fatal error: variable 'i' set but not used [-Wunused-but-set-variable]
# for (uint8_t i = 0;; i++)
CXXFLAGS:append:libc-musl:toolchain-clang = " -Wno-error=unused-but-set-variable"
EXTRA_OECMAKE += "\
-DOT_THREAD_VERSION=1.1 \
-DOTBR_INFRA_IF_NAME=wlan0 \
-DOTBR_BACKBONE_ROUTER=OFF \
-DOTBR_DUA_ROUTING=OFF \
-DOT_DUA=OFF \
-DOT_MLR=OFF \
"
RDEPENDS:${PN} += "ipset"
The patch mentionned in the recipe changes the file third_party/openthread/CMakeLists.txt to its exact copy of the file at sha1 110eb2507caa2fbc9b10935d37f78f6280de1086 in the ot-br-posix git repo. I attached it below.
Best regards,
--JM
2022-12-05 3:33 AM
Hi JM,
Thanks for your solution, I will try.
Best Regards
Frank