2022-08-01 12:04 AM
I need to store a password for encryption in otp registers. I configured device tree in tfa:
&bsec{
status = "okay";
secure-status = "okay";
enc_pass: enc_pass@0x170 {
reg = <0x170 0x10>;
st,non-secure-otp;
};
};
&nvmem_layout {
nvmem-cells = <&enc_pass>;
nvmem-cell-names = "enc_pass";
};
And in uboot and kernel:
&bsec{
status = "okay";
enc_pass: enc_pass@0x170 {
reg = <0x170 0x10>;
st,non-secure-otp;
};
};
NVMEM is configured in kernel defconfig. I can read and write to set otp register in uboot, but i cant read data in linux.
I tried this:
hexdump -C -v /sys/bus/nvmem/devices/stm32-romem0/nvmem
and
dd if=/sys/bus/nvmem/devices/stm32-romem0/nvmem of=/tmp/file
And i have that error:
stm32-romem 5c005000.efuse: Can't read data32 (-5)
hexdump: /sys/bus/nvmem/devices/stm32-romem0/nvmem: Input/output error
Solved! Go to Solution.
2022-08-02 7:21 AM
Hi MJerm.1 (Community Member)
If you are using OpenSTLinux DV3.1 then you should point to the previous wiki version:
Using the DV3.1 version, and the wiki 3.1, I can read upper OTP from linux as OTP57 is by default unprotected in the BSEC on DK2 board.
root@stm32mp1:~# dd if=/sys/bus/nvmem/devices/stm32-romem0/nvmem of=/tmp/file sk
ip=57 bs=4 count=2 status=none
root@stm32mp1:~# hexdump -C -v /tmp/file
00000000 00 80 e1 42 7c d1 00 00 |...B|...|
Also, no issues found with the starter package DV4.0 /OP-TEE image and the current wiki, with the hexdump command.
root@stm32mp1:~# hexdump -C -v /sys/bus/nvmem/devices/stm32-romem0/nvmem
00000000 17 00 00 00 80 80 00 00 00 00 20 a0 00 00 00 00 |.......... .....|
00000010 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000020 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000030 ed f0 f5 7c 2a 00 34 00 18 51 38 34 38 32 38 36 |...|*.4..Q848286|
00000040 e1 75 95 12 65 13 31 3b 40 01 85 7a 1a 14 bd 06 |.u..e.1;@..z....|
00000050 3b 00 f2 5d 00 00 00 00 00 00 00 00 6e 30 16 40 |;..]........n0.@|
00000060 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000070 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000080 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000090 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
000000a0 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
000000b0 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
000000c0 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
000000d0 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
000000e0 00 00 00 00 00 80 e1 42 7c ed 00 00 02 43 72 12 |.......B|....Cr.|
000000f0 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000100 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000110 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000120 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000130 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000140 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000150 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000160 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000170 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000180
After unprotecting all the upper OTP...
root@stm32mp1:~# hexdump -C -v /sys/bus/nvmem/devices/stm32-romem0/nvmem
00000000 17 00 00 00 80 80 00 00 00 00 20 a0 00 00 00 00 |.......... .....|
00000010 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000020 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000030 ed f0 f5 7c 2a 00 34 00 18 51 38 34 38 32 38 36 |...|*.4..Q848286|
00000040 e1 75 95 12 65 13 31 3b 40 01 85 7a 1a 14 bd 06 |.u..e.1;@..z....|
00000050 3b 00 f2 5d 00 00 00 00 00 00 00 00 6e 30 16 40 |;..]........n0.@|
00000060 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000070 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000080 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000090 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
000000a0 4d 4c 9b a0 00 ba 21 1d 92 89 ac fb 5a a4 0f 28 |ML....!.....Z..(|
000000b0 49 8f 2f b0 8d 8d 2c bd c6 39 c1 af df ac e7 7a |I./...,..9.....z|
000000c0 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
000000d0 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
000000e0 00 00 00 00 00 80 e1 42 7c ed 00 00 00 00 00 00 |.......B|.......|
000000f0 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000100 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000110 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000120 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000130 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000140 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000150 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000160 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000170 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000180
2022-08-02 7:21 AM
Hi MJerm.1 (Community Member)
If you are using OpenSTLinux DV3.1 then you should point to the previous wiki version:
Using the DV3.1 version, and the wiki 3.1, I can read upper OTP from linux as OTP57 is by default unprotected in the BSEC on DK2 board.
root@stm32mp1:~# dd if=/sys/bus/nvmem/devices/stm32-romem0/nvmem of=/tmp/file sk
ip=57 bs=4 count=2 status=none
root@stm32mp1:~# hexdump -C -v /tmp/file
00000000 00 80 e1 42 7c d1 00 00 |...B|...|
Also, no issues found with the starter package DV4.0 /OP-TEE image and the current wiki, with the hexdump command.
root@stm32mp1:~# hexdump -C -v /sys/bus/nvmem/devices/stm32-romem0/nvmem
00000000 17 00 00 00 80 80 00 00 00 00 20 a0 00 00 00 00 |.......... .....|
00000010 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000020 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000030 ed f0 f5 7c 2a 00 34 00 18 51 38 34 38 32 38 36 |...|*.4..Q848286|
00000040 e1 75 95 12 65 13 31 3b 40 01 85 7a 1a 14 bd 06 |.u..e.1;@..z....|
00000050 3b 00 f2 5d 00 00 00 00 00 00 00 00 6e 30 16 40 |;..]........n0.@|
00000060 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000070 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000080 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000090 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
000000a0 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
000000b0 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
000000c0 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
000000d0 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
000000e0 00 00 00 00 00 80 e1 42 7c ed 00 00 02 43 72 12 |.......B|....Cr.|
000000f0 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000100 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000110 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000120 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000130 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000140 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000150 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000160 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000170 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000180
After unprotecting all the upper OTP...
root@stm32mp1:~# hexdump -C -v /sys/bus/nvmem/devices/stm32-romem0/nvmem
00000000 17 00 00 00 80 80 00 00 00 00 20 a0 00 00 00 00 |.......... .....|
00000010 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000020 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000030 ed f0 f5 7c 2a 00 34 00 18 51 38 34 38 32 38 36 |...|*.4..Q848286|
00000040 e1 75 95 12 65 13 31 3b 40 01 85 7a 1a 14 bd 06 |.u..e.1;@..z....|
00000050 3b 00 f2 5d 00 00 00 00 00 00 00 00 6e 30 16 40 |;..]........n0.@|
00000060 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000070 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000080 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000090 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
000000a0 4d 4c 9b a0 00 ba 21 1d 92 89 ac fb 5a a4 0f 28 |ML....!.....Z..(|
000000b0 49 8f 2f b0 8d 8d 2c bd c6 39 c1 af df ac e7 7a |I./...,..9.....z|
000000c0 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
000000d0 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
000000e0 00 00 00 00 00 80 e1 42 7c ed 00 00 00 00 00 00 |.......B|.......|
000000f0 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000100 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000110 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000120 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000130 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000140 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000150 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000160 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000170 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................|
00000180
2022-08-03 10:48 PM
Thank you, it helped, I didn't notice that the version had already changed
2022-08-04 1:16 AM
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'