2022-09-29 10:57 PM
I want to pass the some parameters to kernel command line.
drm.edid_firmware=edid/1280x800.bin
I tried to use "bootargs" environment of uboot.
env set bootargs "drm.edid_firmware=edid/1280x800.bin"
But, Not working as I expect.
I couldn't find my parameter in kernel command line.
below is dmesg log.
Kernel command line: root=PARTUUID=491f6117-415d-4f53-88c9-6e0de54deac6 rootwait rw console=ttySTM0,115200
below is /proc/cmdline log.
root@stm32mp15:~# cat /proc/cmdline
root=PARTUUID=491f6117-415d-4f53-88c9-6e0de54deac6 rootwait rw console=ttySTM0,115200
How to pass the kernel command line parameters on uboot?
thanks in advance.
Solved! Go to Solution.
2022-09-30 12:39 AM
Hello @hochul yoo ,
In the ST environment, the U-boot got the kernel bootargs from an extlinux.conf. This information can be found in the wiki: https://wiki.st.com/stm32mpu/wiki/U-Boot_overview#Generic_Distro_configuration
You can see the name of this file during the boot of your board, in the U-Boot traces:
mmc0 is current device
Scanning mmc 0:8...
Found /mmc0_extlinux/stm32mp157f-dk2_extlinux.conf
Retrieving file: /mmc0_extlinux/stm32mp157f-dk2_extlinux.conf
In this file, the several boot modes are listed and you can see the kernel bootargs associated to these configurations:
root@stm32mp1:/# cat ./boot/mmc0_extlinux/stm32mp157f-dk2_extlinux.conf
# Generic Distro Configuration file generated by OpenEmbedded
menu title Select the boot mode
MENU BACKGROUND /splash_portrait.bmp
TIMEOUT 20
DEFAULT OpenSTLinux
LABEL OpenSTLinux
KERNEL /uImage
FDTDIR /
INITRD /st-image-resize-initrd
APPEND root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=${console},${baudrate}
LABEL stm32mp157f-dk2-a7-examples
KERNEL /uImage
FDT /stm32mp157f-dk2-a7-examples.dtb
INITRD /st-image-resize-initrd
APPEND root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=${console},${baudrate}
LABEL stm32mp157f-dk2-m4-examples
KERNEL /uImage
FDT /stm32mp157f-dk2-m4-examples.dtb
INITRD /st-image-resize-initrd
APPEND root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=${console},${baudrate}
Modify the bootargs
To modify this file, you can edit it once you are in the linux by doing an edit with "vi".
Or you can follow this page that explains several way to edit the extlinux.conf: https://wiki.st.com/stm32mpu/wiki/How_to_use_the_kernel_dynamic_debug#Debug_messages_during_boot_process
Hope it helps,
Best Regards,
Kevin
2022-09-30 12:39 AM
Hello @hochul yoo ,
In the ST environment, the U-boot got the kernel bootargs from an extlinux.conf. This information can be found in the wiki: https://wiki.st.com/stm32mpu/wiki/U-Boot_overview#Generic_Distro_configuration
You can see the name of this file during the boot of your board, in the U-Boot traces:
mmc0 is current device
Scanning mmc 0:8...
Found /mmc0_extlinux/stm32mp157f-dk2_extlinux.conf
Retrieving file: /mmc0_extlinux/stm32mp157f-dk2_extlinux.conf
In this file, the several boot modes are listed and you can see the kernel bootargs associated to these configurations:
root@stm32mp1:/# cat ./boot/mmc0_extlinux/stm32mp157f-dk2_extlinux.conf
# Generic Distro Configuration file generated by OpenEmbedded
menu title Select the boot mode
MENU BACKGROUND /splash_portrait.bmp
TIMEOUT 20
DEFAULT OpenSTLinux
LABEL OpenSTLinux
KERNEL /uImage
FDTDIR /
INITRD /st-image-resize-initrd
APPEND root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=${console},${baudrate}
LABEL stm32mp157f-dk2-a7-examples
KERNEL /uImage
FDT /stm32mp157f-dk2-a7-examples.dtb
INITRD /st-image-resize-initrd
APPEND root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=${console},${baudrate}
LABEL stm32mp157f-dk2-m4-examples
KERNEL /uImage
FDT /stm32mp157f-dk2-m4-examples.dtb
INITRD /st-image-resize-initrd
APPEND root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=${console},${baudrate}
Modify the bootargs
To modify this file, you can edit it once you are in the linux by doing an edit with "vi".
Or you can follow this page that explains several way to edit the extlinux.conf: https://wiki.st.com/stm32mpu/wiki/How_to_use_the_kernel_dynamic_debug#Debug_messages_during_boot_process
Hope it helps,
Best Regards,
Kevin
2022-09-30 12:46 AM
Hello @hochul yoo ,
I just saw that you already solved your problem in another topic: https://community.st.com/s/question/0D53W00001pumzNSAQ/the-way-of-specify-an-edid-data-to-display-dual-screen-
Anyway, this question will maybe help someone else in the community.
Feel free to set my previous message as Best Answer.
Best Regards,
Kevin
2022-09-30 1:11 AM
Thanks for your answer.
I have one more question !!!
I modified it by myself with the vi editor now, but
When I build my own distribution package, I want to add this kernel parameter by default.
What part of the wiki can I refer to?
2022-09-30 2:13 AM
Hello again @hochul yoo ,
You can have a look at this question: https://community.st.com/s/question/0D53W000014zXu5SAE/change-uboot-kernel-command-line
The file that generates the extlinux.conf is "openembedded-core/meta/classes/uboot-extlinux-config.bbclass"
The variable UBOOT_EXTLINUX_KERNEL_ARGS contains the bootargs. But it is recommended to not modify this variable here, but modify the one from the machine configuration located in line 17 of the file:
./meta-st/meta-st-stm32mp/conf/machine/include/st-machine-extlinux-config-stm32mp.inc
meta-st/meta-st-stm32mp/conf/machine/include/st-machine-extlinux-config-stm32mp.inc:17:UBOOT_EXTLINUX_KERNEL_ARGS ?= "rootwait rw"
Hope it helps you,
Best Regards,
Kevin