2021-02-18 12:39 AM
the microcontroller receives a total of 4 bytes of data every 50 µs via SPI. each Two bytes form a value, which is represented as a float with 16 bits.
how can i join two bytes into a 16-bit float?
float v_beta_d_star = 0.0f;
float v_beta_q_star = 0.0f;
float v_beta_d_star = (spi_values[0] << 😎 | (spi_values[0] & 0xFF);
float v_beta_d_star = (spi_values[1] << 😎 | (spi_values[1] & 0xFF);
2021-02-18 12:54 AM
floats have 32 bit, and they dont store data the same way as integers or byte variables.
I dont know if this will help you but:
from two byte variables to one uint16_t;
memcpy(&first16bitvariable,&spi_values[0],2);
memcpy(&second16bitvariable,&spi_values[2],2);
once you have the 16bit integers you can use them to do some maths with floats
2021-02-18 03:11 AM
Nitpicking:
memcpy does not care for byte order in your spi data. With 16bitvariable = spi_values[0] | spi_values[1] << 8 or 16bitvariable = spi_values[1] | spi_values[0] << 8 you can care for byte order.
2021-02-18 03:17 AM
Floating point formats are standardized, see here: https://en.wikipedia.org/wiki/IEEE_754
For endianess, check the datasheet of the SPI slave you receive the values from.
Alternatively, the datasheet should define the number format used.