cancel
Showing results for 
Search instead for 
Did you mean: 

How to compile kernel in Yocto to contain rtl8192cu driver?

ShawnHymel
Associate II

I have an old Edimax EW-7811Un that I am trying to get working on the STM32MP157D-DK1. I have installed Yocto along with poky and the meta-st-stm32mp BSP layer. I do not want to use OpenSTLinux right now.

I configured the kernel with

bitbake -c menuconfig virtual/kernel 

and made sure the following kernel modules were enabled:

  • Networking support > Networking options (following should be enabled):
    • [*] TCP/IP networking
      • [*] IP: kernel level autoconfiguration
        • [*] IP: DHCP support
        • [*] IP: BOOTP support
        • [*] IP: RARP support
      • <*> The IPv6 protocol
  • Networking support > Wireless
    • <M> cfg80211 - wireless configuration API
    • [*] cfg80211 wireless extensions compatibility (for compatibility with some older tools, e.g. get iwconfig to talk to device)
    • <M> Generic IEEE 802.11 Networking Stack (mac80211)
    • [*] Minstrel (for rate control in 802.11)
  • Device Drivers > USB support, make sure USB Host is enabled:
    • <*> Support for Host-side USB
    • [*] Enable USB persist by default
  • Device Drivers> Network device support > Wireless LAN
    • <M> Realtek rtlwifi family of devices
      • <M> Realtek RTL8192CU/RTL8188CU USB Wireless Network Adapter
      • [*] Debugging output for rtlwifi driver family

I added the following line to the end of conf/local.conf:

IMAGE_INSTALL += “linux-firmware-rtl8192cu�?

I built an image with:

bitbake core-image-minimal

However, it does not seem that the rtl8192cu module was included. I checked the manifest file with:

cat tmp/deploy/images/stm32mp1/core-image-minimal-stm32mp1.manifest | grep rtl

Nothing shows up, which should indicate that the rtl8192cu module was not included in the build, right?

I tried flashing the image to an SD card and booted up the board. I plug in the USB WiFi dongle and dmesg does not show that the driver is loading.

What am I missing to make this driver work?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Kevin HUBER
ST Employee

Hi @ShawnHymel​ 

I don't know if you are still facing this problem, but maybe your issue is related to your kernel configuration.

In your linux configuration, the driver RTL8192CU is enabled as a Module (M means module), so you have to load the module.ko manually.

Device Drivers> Network device support > Wireless LAN

  • <M> Realtek rtlwifi family of devices
    • <M> Realtek RTL8192CU/RTL8188CU USB Wireless Network Adapter
    • [*] Debugging output for rtlwifi driver family

You can check if your module is loaded by using the command:

lsmod | grep "rtl"

To build and "load" the driver by default, you have to enable it in the linux configuration, please switch:

  • <M> Realtek RTL8192CU/RTL8188CU USB Wireless Network Adapter

to

  • <*> Realtek RTL8192CU/RTL8188CU USB Wireless Network Adapter

Hope it help,

Regards,

Kevin

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Kevin HUBER
ST Employee

Hi @ShawnHymel​ 

I don't know if you are still facing this problem, but maybe your issue is related to your kernel configuration.

In your linux configuration, the driver RTL8192CU is enabled as a Module (M means module), so you have to load the module.ko manually.

Device Drivers> Network device support > Wireless LAN

  • <M> Realtek rtlwifi family of devices
    • <M> Realtek RTL8192CU/RTL8188CU USB Wireless Network Adapter
    • [*] Debugging output for rtlwifi driver family

You can check if your module is loaded by using the command:

lsmod | grep "rtl"

To build and "load" the driver by default, you have to enable it in the linux configuration, please switch:

  • <M> Realtek RTL8192CU/RTL8188CU USB Wireless Network Adapter

to

  • <*> Realtek RTL8192CU/RTL8188CU USB Wireless Network Adapter

Hope it help,

Regards,

Kevin

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Kevin HUBER
ST Employee

Hi,

You can find more information about the menuconfig on the wiki: https://wiki.st.com/stm32mpu/wiki/Menuconfig_or_how_to_configure_kernel#Menuconfig_and_Developer_Package

Regards,

Kevin

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.