2020-01-14 08:29 AM
According to the documentation of the EV1 eval board:
"The STM32MP157xAA3 also drives a sub system reset, SUB_NRST signal on PD10 IO, to the peripherals: USB Host Hub, MFX, Ethernet, and RGB_LTDC connector."
Is this signal generated automatically by the STM32MP157? Is it software controlled? If the latter, is this implemented in OpenSTLinux images by default?
Thanks,
Guillermo
Solved! Go to Solution.
2020-01-16 01:11 AM
Hi Guillermo
The SUB_NRST signal is software controlled. But there's no default implementation in OpenSTLinux.
BR,
Milan
2020-01-16 01:11 AM
Hi Guillermo
The SUB_NRST signal is software controlled. But there's no default implementation in OpenSTLinux.
BR,
Milan
2020-01-16 01:18 AM
Clear, thank you!