2022-01-11 2:51 AM
I have built a test program from the two examples PWR_STOP_CoPro and LPTIM_PulseCounter. With the LPTIM_PulseCounter I changed the CounterSource to LPTIM_COUNTERSOURCE_INTERNAL and adjusted the priority HAL_NVIC_SetPriority (LPTIM2_IRQn, 0, 0);
Both programs run as expected only when I start the timer HAL_LPTIM_TimeOut_Start_IT (& hlptim2, 0xFFFF, 0x7000) and then go to STOP Mode HAL_PWR_EnterSTOPMode (PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI); the M4 core does not wake up by the LP Timer interrupt, but an EXTI interrupt lets it wake up.
Can someone tell me what I might have overlooked?
2022-01-14 3:40 AM
Hi @Dirk Höning ,
As per stipulated in Ref man and in wiki Coprocessor power management - stm32mpu wakeup can only be done with EXTI.
EXTI mapped to the LPTIM instance is defined in Linux Device Tree.
Olivier
2022-01-21 3:38 AM
Hi Olivier,
thanks for the reply. It is hard for us to figure out how to map the LPTIM to the EXTI events in the Device-Tree. Could you provide an example for this configuration?
Best regards
Dirk