2022-08-11 12:36 AM
When I use cmake,
/opt/st/stm32mp1/4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/sysroots/x86_64-ostl_sdk-linux/usr/share/cmake-3.22/Modules/CMakeTestCXXCompiler.cmake:62: error: The C++ compiler "/opt/st/stm32mp1/4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/sysroots/x86_64-ostl_sdk-linux/usr/bin/arm-ostl-linux-gnueabi/arm-ostl-linux-gnueabi-g++" is not able to compile a simple test program. It fails with the following output: Change Dir: /home/zxb/qt_proj/build-untitled1-Stm32mp1-Debug/CMakeFiles/CMakeTmp Run Build Command(s):/opt/st/stm32mp1/4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/sysroots/x86_64-ostl_sdk-linux/usr/bin/ninja cmTC_1f845 && [1/2] Building CXX object CMakeFiles/cmTC_1f845.dir/testCXXCompiler.cxx.o [2/2] Linking CXX executable cmTC_1f845 FAILED: cmTC_1f845 : && /opt/st/stm32mp1/4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/sysroots/x86_64-ostl_sdk-linux/usr/bin/arm-ostl-linux-gnueabi/arm-ostl-linux-gnueabi-g++ --sysroot=/opt/st/stm32mp1/4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi -O2 -pipe -g -feliminate-unused-debug-types -Wl,-O1 -Wl,--hash-style=gnu -Wl,--as-needed CMakeFiles/cmTC_1f845.dir/testCXXCompiler.cxx.o -o cmTC_1f845 && : /opt/st/stm32mp1/4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/sysroots/x86_64-ostl_sdk-linux/usr/libexec/arm-ostl-linux-gnueabi/gcc/arm-ostl-linux-gnueabi/11.2.0/real-ld: error: cmTC_1f845 uses VFP register arguments, CMakeFiles/cmTC_1f845.dir/testCXXCompiler.cxx.o does not /opt/st/stm32mp1/4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/sysroots/x86_64-ostl_sdk-linux/usr/libexec/arm-ostl-linux-gnueabi/gcc/arm-ostl-linux-gnueabi/11.2.0/real-ld: failed to merge target specific data of file CMakeFiles/cmTC_1f845.dir/testCXXCompiler.cxx.o collect2: error: ld returned 1 exit status ninja: build stopped: subcommand failed.
I got this...How can I configure Qtcreator to work normally?
2022-09-01 2:47 AM
Hi @zxiao.4 ,
Not sure it will fix your problem but please update to 4.0.2 release and let us know if you still have issue
OpenSTLinux Distribution patch release V4.0.2 is available
Olivier