cancel
Showing results for 
Search instead for 
Did you mean: 

question about ecosystem4

zqizh.1
Associate II

Hi,

I follow "https://wiki.st.com/stm32mpu/wiki/PMIC_hardware_components#Support_in_Cortex-A7_Secure" can port the ecosystem 3.0 on the kit "stm32mp157c-odyssey" successfully, but fail to port the ecosystem4.0.

The error log is :

"

 14:13:55 : Start Embedded Flashing service

 14:13:55 : Memory Programming ...

 14:13:55 : Opening and parsing file: tf-a-stm32mp157c-odyssey-usb.stm32

 14:13:55 :  File     : tf-a-stm32mp157c-odyssey-usb.stm32

 14:13:55 :  Size     : 225.76 KB 

 14:13:55 :  Partition ID : 0x01 

 14:13:55 : Download in Progress:

 14:13:56 : File download complete

 14:13:56 : Time elapsed during download operation: 00:00:01.064

 14:13:56 : RUNNING Program ... 

 14:13:56 :  PartID:   :0x01 

 14:14:14 : Error: Start operation failed at partition 0x01

 14:14:14 : Error: TSV flashing service failed

 14:14:14 : Warning: Connection to device 0x500 is lost

 14:14:14 : Disconnected from device.

"

"

PANIC at PC : 0x2fff1a17

Exception mode=0x00000016 at: 0x2fff1a17

"

Please advise what difference between the ecosystem4.0 to ecosystem 3.0 can cause I port the ecosystem4.0 to kit "stm32mp157c-odyssey" fail.

The attachment is the compiler log, please advise whether the log is correct. My PC OS is UBUNTU20.04.

Thanks,

QiZhang

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Olivier GALLIEN
ST Employee

Hi @zqizh.1​ ,

Did you try to reach Seeed support ?

I'm quite sure they already have or will soon provide ODYSSEY support with Ecosystem 4.

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Olivier GALLIEN
ST Employee

Hi @zqizh.1​ ,

Did you try to reach Seeed support ?

I'm quite sure they already have or will soon provide ODYSSEY support with Ecosystem 4.

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.