2022-05-10 1:43 AM
Hi
I try to implement a virtual UART communication between the A7 and the M4 on a STM32MP157 device based on OpenAMP. I used the OpenAMP_TTY_echo example from the cube firmware package and adapted it to my own board. The virtual UART is working. But there are log commands in the example like " log_info("Virtual UART0 OpenAMP-rpmsg channel creation\r\n");" and this messages are not printed.
Is there a way to print this logs on the Linux terminal that is connected to the A7 or to forward it to an additional UART or something similar?
Thanks.
2022-05-11 12:20 AM
Hello @Corono ,
These log_info messages are not directly printed in your Linux console but you can get these messages with some commands from Linux side.
You can find information on this wiki page : https://wiki.st.com/stm32mpu/wiki/Linux_remoteproc_framework_overview
Hope that it will help you.
Regards.
Erwan.