2021-02-01 8:54 PM
Hi.... there
Hope you all are doing well
From past few days, I'm playing with STM32MP1
I need to integrate the Quectel EG25G module with the image having ppp functionality
To do so, i have enable ppp support at Make-menuconfig and build the image
Now the problem is, after building the image from scratch, i haven't found the directory /etc/ppp
Even i have also try with the installation from apt-get
But unfortunately, it's not working
Any suggestions ?
Thanks
2021-02-02 4:27 AM
Are you using a correct recipe?
2022-05-10 2:09 PM
Do you have any progress?