cancel
Showing results for 
Search instead for 
Did you mean: 

Error parsing recipes using meta-st-openstlinux in Yocto

obedPH
Associate III

Hello,

 

I am developing a custom image using the layer meta-st-stm32mp in the mickledore branch, until that point, there are no problems.

The problem is, since I want ti install the meta-st-x-linux-ai layer, I need to install meta-st-openstlinux first, which has several layer dependencies such as meta-qt5, and other layers.

 

The problem I am having is, once I add the meta-st-openstlinux, the process stops, it does not even initiallizes the tasks, because the parsing process does not succeed.

This is the local.conf (I did not add the recipes because I thought maybe some of my recipes did generate the problem):

 

# This file is your local configuration file and is where all local user settings # are placed. The comments in this file give some guide to the options a new user # to the system might want to change but pretty much any configuration option can # be set in this file. More adventurous users can look at # local.conf.sample.extended which contains other examples of configuration which # can be placed in this file but new users likely won't need any of them # initially. # # Lines starting with the '#' character are commented out and in some cases the # default values are provided as comments to show people example syntax. Enabling # the option is a question of removing the # character and making any change to the # variable as required. # # Machine Selection # # You need to select a specific machine to target the build with. There are a selection # of emulated machines available which can boot and run in the QEMU emulator: # #MACHINE ?= "qemuarm" #MACHINE ?= "qemuarm64" #MACHINE ?= "qemumips" #MACHINE ?= "qemumips64" #MACHINE ?= "qemuppc" #MACHINE ?= "qemux86" #MACHINE ?= "qemux86-64" # # There are also the following hardware board target machines included for # demonstration purposes: # #MACHINE ?= "beaglebone-yocto" #MACHINE ?= "genericx86" #MACHINE ?= "genericx86-64" #MACHINE ?= "edgerouter" # # This sets the default machine to be qemux86-64 if no other machine is selected: # MACHINE ??= "qemux86-64" MACHINE = "stm32mp1" # # Where to place downloads # # During a first build the system will download many different source code tarballs # from various upstream projects. This can take a while, particularly if your network # connection is slow. These are all stored in DL_DIR. When wiping and rebuilding you # can preserve this directory to speed up this part of subsequent builds. This directory # is safe to share between multiple builds on the same machine too. # # The default is a downloads directory under TOPDIR which is the build directory. # #DL_DIR ?= "${TOPDIR}/downloads" # # Where to place shared-state files # # BitBake has the capability to accelerate builds based on previously built output. # This is done using "shared state" files which can be thought of as cache objects # and this option determines where those files are placed. # # You can wipe out TMPDIR leaving this directory intact and the build would regenerate # from these files if no changes were made to the configuration. If changes were made # to the configuration, only shared state files where the state was still valid would # be used (done using checksums). # # The default is a sstate-cache directory under TOPDIR. # #SSTATE_DIR ?= "${TOPDIR}/sstate-cache" # # Where to place the build output # # This option specifies where the bulk of the building work should be done and # where BitBake should place its temporary files and output. Keep in mind that # this includes the extraction and compilation of many applications and the toolchain # which can use Gigabytes of hard disk space. # # The default is a tmp directory under TOPDIR. # #TMPDIR = "${TOPDIR}/tmp" # # Default policy config # # The distribution setting controls which policy settings are used as defaults. # The default value is fine for general Yocto project use, at least initially. # Ultimately when creating custom policy, people will likely end up subclassing # these defaults. # DISTRO = "poky" # As an example of a subclass there is a "bleeding" edge policy configuration # where many versions are set to the absolute latest code from the upstream # source control systems. This is just mentioned here as an example, its not # useful to most new users. # DISTRO ?= "poky-bleeding" # # Package Management configuration # # This variable lists which packaging formats to enable. Multiple package backends # can be enabled at once and the first item listed in the variable will be used # to generate the root filesystems. # Options are: # - 'package_deb' for debian style deb files # - 'package_ipk' for ipk files are used by opkg (a debian style embedded package manager) # - 'package_rpm' for rpm style packages # E.g.: PACKAGE_CLASSES ?= "package_rpm package_deb package_ipk" # We default to rpm: PACKAGE_CLASSES = "package_rpm" # # SDK target architecture # # This variable specifies the architecture to build SDK items for and means # you can build the SDK packages for architectures other than the machine you are # running the build on (i.e. building i686 packages on an x86_64 host). # Supported values are i686, x86_64, aarch64 #SDKMACHINE ?= "i686" # # Extra image configuration defaults # # The EXTRA_IMAGE_FEATURES variable allows extra packages to be added to the generated # images. Some of these options are added to certain image types automatically. The # variable can contain the following options: # "dbg-pkgs" - add -dbg packages for all installed packages # (adds symbol information for debugging/profiling) # "src-pkgs" - add -src packages for all installed packages # (adds source code for debugging) # "dev-pkgs" - add -dev packages for all installed packages # (useful if you want to develop against libs in the image) # "ptest-pkgs" - add -ptest packages for all ptest-enabled packages # (useful if you want to run the package test suites) # "tools-sdk" - add development tools (gcc, make, pkgconfig etc.) # "tools-debug" - add debugging tools (gdb, strace) # "eclipse-debug" - add Eclipse remote debugging support # "tools-profile" - add profiling tools (oprofile, lttng, valgrind) # "tools-testapps" - add useful testing tools (ts_print, aplay, arecord etc.) # "debug-tweaks" - make an image suitable for development # e.g. ssh root access has a blank password # There are other application targets that can be used here too, see # meta/classes/image.bbclass and meta/classes/core-image.bbclass for more details. # We default to enabling the debugging tweaks. EXTRA_IMAGE_FEATURES = "debug-tweaks" # # Additional image features # # The following is a list of additional classes to use when building images which # enable extra features. Some available options which can be included in this variable # are: # - 'buildstats' collect build statistics USER_CLASSES = "buildstats" # # Runtime testing of images # # The build system can test booting virtual machine images under qemu (an emulator) # after any root filesystems are created and run tests against those images. It can also # run tests against any SDK that are built. To enable this uncomment these lines. # See classes/test{image,sdk}.bbclass for further details. #IMAGE_CLASSES += "testimage testsdk" #TESTIMAGE_AUTO:qemuall = "1" # # Interactive shell configuration # # Under certain circumstances the system may need input from you and to do this it # can launch an interactive shell. It needs to do this since the build is # multithreaded and needs to be able to handle the case where more than one parallel # process may require the user's attention. The default is iterate over the available # terminal types to find one that works. # # Examples of the occasions this may happen are when resolving patches which cannot # be applied, to use the devshell or the kernel menuconfig # # Supported values are auto, gnome, xfce, rxvt, screen, konsole (KDE 3.x only), none # Note: currently, Konsole support only works for KDE 3.x due to the way # newer Konsole versions behave #OE_TERMINAL = "auto" # By default disable interactive patch resolution (tasks will just fail instead): PATCHRESOLVE = "noop" # # Disk Space Monitoring during the build # # Monitor the disk space during the build. If there is less that 1GB of space or less # than 100K inodes in any key build location (TMPDIR, DL_DIR, SSTATE_DIR), gracefully # shutdown the build. If there is less than 100MB or 1K inodes, perform a hard halt # of the build. The reason for this is that running completely out of space can corrupt # files and damages the build in ways which may not be easily recoverable. # It's necessary to monitor /tmp, if there is no space left the build will fail # with very exotic errors. BB_DISKMON_DIRS ??= "\ STOPTASKS,${TMPDIR},1G,100K \ STOPTASKS,${DL_DIR},1G,100K \ STOPTASKS,${SSTATE_DIR},1G,100K \ STOPTASKS,/tmp,100M,100K \ HALT,${TMPDIR},100M,1K \ HALT,${DL_DIR},100M,1K \ HALT,${SSTATE_DIR},100M,1K \ HALT,/tmp,10M,1K" # # Shared-state files from other locations # # As mentioned above, shared state files are prebuilt cache data objects which can be # used to accelerate build time. This variable can be used to configure the system # to search other mirror locations for these objects before it builds the data itself. # # This can be a filesystem directory, or a remote url such as https or ftp. These # would contain the sstate-cache results from previous builds (possibly from other # machines). This variable works like fetcher MIRRORS/PREMIRRORS and points to the # cache locations to check for the shared objects. # NOTE: if the mirror uses the same structure as SSTATE_DIR, you need to add PATH # at the end as shown in the examples below. This will be substituted with the # correct path within the directory structure. #SSTATE_MIRRORS ?= "\ #file://.* https://someserver.tld/share/sstate/PATH;downloadfilename=PATH \ #file://.* file:///some/local/dir/sstate/PATH" # # Yocto Project SState Mirror # # The Yocto Project has prebuilt artefacts available for its releases, you can enable # use of these by uncommenting the following lines. This will mean the build uses # the network to check for artefacts at the start of builds, which does slow it down # equally, it will also speed up the builds by not having to build things if they are # present in the cache. It assumes you can download something faster than you can build it # which will depend on your network. # Note: For this to work you also need hash-equivalence passthrough to the matching server # #BB_HASHSERVE_UPSTREAM = "hashserv.yocto.io:8687" #SSTATE_MIRRORS ?= "file://.* http://sstate.yoctoproject.org/all/PATH;downloadfilename=PATH" # # Qemu configuration # # By default native qemu will build with a builtin VNC server where graphical output can be # seen. The line below enables the SDL UI frontend too. PACKAGECONFIG:append:pn-qemu-system-native = " sdl" # By default libsdl2-native will be built, if you want to use your host's libSDL instead of # the minimal libsdl built by libsdl2-native then uncomment the ASSUME_PROVIDED line below. #ASSUME_PROVIDED += "libsdl2-native" # You can also enable the Gtk UI frontend, which takes somewhat longer to build, but adds # a handy set of menus for controlling the emulator. #PACKAGECONFIG:append:pn-qemu-system-native = " gtk+" # # Hash Equivalence # # Enable support for automatically running a local hash equivalence server and # instruct bitbake to use a hash equivalence aware signature generator. Hash # equivalence improves reuse of sstate by detecting when a given sstate # artifact can be reused as equivalent, even if the current task hash doesn't # match the one that generated the artifact. # # A shared hash equivalent server can be set with "<HOSTNAME>:<PORT>" format # #BB_HASHSERVE = "auto" #BB_SIGNATURE_HANDLER = "OEEquivHash" # # Memory Resident Bitbake # # Bitbake's server component can stay in memory after the UI for the current command # has completed. This means subsequent commands can run faster since there is no need # for bitbake to reload cache files and so on. Number is in seconds, after which the # server will shut down. # #BB_SERVER_TIMEOUT = "60" # CONF_VERSION is increased each time build/conf/ changes incompatibly and is used to # track the version of this file when it was generated. This can safely be ignored if # this doesn't mean anything to you. CONF_VERSION = "2"
View more

 

 

This is my bblayer file

 

# POKY_BBLAYERS_CONF_VERSION is increased each time build/conf/bblayers.conf # changes incompatibly POKY_BBLAYERS_CONF_VERSION = "2" BBPATH = "${TOPDIR}" BBFILES ?= "" BBLAYERS ?= " \ /home/obed/Documents/Yocto/poky/meta \ /home/obed/Documents/Yocto/poky/meta-poky \ /home/obed/Documents/Yocto/poky/meta-yocto-bsp \ /home/obed/Documents/Yocto/meta-openembedded/meta-oe \ /home/obed/Documents/Yocto/meta-openembedded/meta-python \ /home/obed/Documents/Yocto/meta-openembedded/meta-networking \ /home/obed/Documents/Yocto/meta-openembedded/meta-gnome \ /home/obed/Documents/Yocto/meta-openembedded/meta-webserver \ /home/obed/Documents/Yocto/meta-openembedded/meta-multimedia \ /home/obed/Documents/Yocto/meta-st-stm32mp \ /home/obed/Documents/Yocto/meta-qt5 \ /home/obed/Documents/Yocto/meta-st-openstlinux \ /home/obed/Documents/Yocto/meta-custom-quoia \ "

 

 

The error I get when I try to run the bitbake command is the next

 

Loading cache: 100% |###########################################################################################| Time: 0:00:00 Loaded 1771 entries from dependency cache. NOTE: /home/obed/Documents/Yocto/meta-st-openstlinux/recipes-st/images/st-image-resize-initrd.bb: ENABLE_PARTITIONS_IMAGE not enabled WARNING: /home/obed/Documents/Yocto/meta-st-openstlinux/recipes-core/systemd/systemd-mount-partitions.bb: Exception during build_dependencies for PARTITIONS_IMAGES[rootfs] WARNING: /home/obed/Documents/Yocto/meta-st-openstlinux/recipes-core/systemd/systemd-mount-partitions.bb: Error during finalise of /home/obed/Documents/Yocto/meta-st-openstlinux/recipes-core/systemd/systemd-mount-partitions.bb ERROR: ExpansionError during parsing /home/obed/Documents/Yocto/meta-st-openstlinux/recipes-core/systemd/systemd-mount-partitions.bb Traceback (most recent call last): File "Var <STM32MP_ROOTFS_IMAGE>", line 1, in <module> bb.data_smart.ExpansionError: Failure expanding variable STM32MP_ROOTFS_IMAGE, expression was ${@[d.getVar('IMAGE_BASENAME'), d.getVar('IMAGE_BASENAME').replace('-%s' % d.getVar('DISTRO'), '')][d.getVar('TARGET_VENDOR') == (d.getVar('STM32MP_TARGETVENDOR') or "")]} which triggered exception AttributeError: 'NoneType' object has no attribute 'replace' The variable dependency chain for the failure is: STM32MP_ROOTFS_IMAGE -> PARTITIONS_IMAGES[rootfs] ERROR: Parsing halted due to errors, see error messages above WARNING: /home/obed/Documents/Yocto/poky/meta/recipes-core/images/core-image-ptest.bb: Error during finalise of virtual:mcextend:gawk:/home/obed/Documents/Yocto/poky/meta/recipes-core/images/core-image-ptest.bb

 

What could be the reason for that?

 

Thank you,

 

Regards

1 ACCEPTED SOLUTION

Accepted Solutions

Hi @obedPH ,
Yes sorry I have just took a diff extract that I kept on a side ..

I am glad to see that it helps you. Do not hesitate to put it as accepted solution as it can help other community members.

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Erwan SZYMANSKI
ST Employee

Hello @obedPH ,
I tried myself to make a such thing one day, and I think I remember what I did for that, please tell me if it works for you or not :

diff --git a/conf/machine/include/st-machine-common-stm32mp.inc b/conf/machine/include/st-machine-common-stm32mp.inc index b21cee6..1fabaa0 100644 --- a/conf/machine/include/st-machine-common-stm32mp.inc +++ b/conf/machine/include/st-machine-common-stm32mp.inc @@ -273,7 +273,8 @@ STM32MP_BOOTFS_LABEL ?= "bootfs" STM32MP_BOOTFS_MOUNTPOINT ?= "/boot" # Proposed value for bootfs is 64MB STM32MP_BOOTFS_SIZE ?= "65536" -STM32MP_ROOTFS_IMAGE ?= "${@[d.getVar('IMAGE_BASENAME'), d.getVar('IMAGE_BASENAME').replace('-%s' % d.getVar('DISTRO'), '')][d.getVar('TARGET_VENDOR') == (d.getVar('STM32MP_TARGETVENDOR') or "")]}" +# STM32MP_ROOTFS_IMAGE ?= "${@[d.getVar('IMAGE_BASENAME'), d.getVar('IMAGE_BASENAME').replace('-%s' % d.getVar('DISTRO'), '')][d.getVar('TARGET_VENDOR') == (d.getVar('STM32MP_TARGETVENDOR') or "")]}" +STM32MP_ROOTFS_IMAGE = "${IMAGE_BASENAME}" STM32MP_ROOTFS_LABEL ?= "rootfs" # Configure the rootfs size with IMAGE_ROOTFS_MAXSIZE variable STM32MP_ROOTFS_SIZE ?= "${IMAGE_ROOTFS_MAXSIZE}"

Please try a such patch and tell me if it solves the issue for you or not.

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
obedPH
Associate III

Hello @Erwan SZYMANSKI 

Thank you for your response, finally the compilation process is starting.

A few details, first, the file is not correct. The file where you should add the patch (if you prefer that option) is conf/machine/include/st-machine-image-partition-stm32mp.inc, and the line don't correspond to the current file, so if you want to apply that patch in the current version of the mickledore branch you need to modify the patch with the git diff command to addapt to the curreent .inc file in the github repository.

However, there is another option where you don't need to apply that patch, you can just add the next line to the local.conf file

STM32MP_ROOTFS_IMAGE = "${IMAGE_BASENAME}"

 I appreciate your help a lot, I've been struggling with that error a long time, thank you so much.

Regards

Hi @obedPH ,
Yes sorry I have just took a diff extract that I kept on a side ..

I am glad to see that it helps you. Do not hesitate to put it as accepted solution as it can help other community members.

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.