2023-09-08 02:01 AM - edited 2023-09-08 02:02 AM
Hi,
We are working on developing a custom board that necessitates the immediate activation of a buzzer with a predefined frequency as soon as the board is powered up. We are exploring the feasibility of utilizing the PWM driver in U-Boot to achieve this functionality.
Can anyone advise if it is possible to configure the U-Boot PWM driver to meet this requirement? Additionally, we are seeking references or guidance regarding the necessary configurations in the U-Boot device tree and source code to accomplish this task effectively.