cancel
Showing results for 
Search instead for 
Did you mean: 

devmem2 not working.I have installed devmem2 in my development board to read the peripheral registers however the command is not working /dev/mem opened however it is showing Error at line 75, file devmem2.c (1) [Operation not permitted]

KS.2
Associate III
 
This discussion is locked. Please start a new topic to ask your question.
16 REPLIES 16
OlivierK
ST Employee

However if you can move to openstlinux v3.0 it will likely solve your issue.

Will try that

we are working on a sip based on stm32mp157c ,we are using a sdk for building the kernel for a developer package the sdk only supports v2.0

is there an sdk that supports v3.0??

the problem.was with the internet connectivity fixed it and installed devmem2 now its working fine

Thank you for your help

Hi OliverK

Is there a way to establish communication with the coprocessor in the stm32mp157c

OlivierK
ST Employee

Hi KS.2 (Community Member)

Please close this topic and open a new one for clarity.

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

For the coprocessor topic this is where to start:

https://wiki.st.com/stm32mpu/wiki/Coprocessor_management_overview